Other Parts Discussed in Thread: CC2538
我的project 是用CC2538作为处理器,读取MEMS sensor 的数据。原理是这样的:
CC2538首先发送一组数据到MEMS通过MOSI线,然后MEMS返回一组数据通过MISO线。
我想用TI的driver library 编程,我修改了他的example 代码,
#include <stdbool.h>
#include <stdint.h>
#include "hw_memmap.h"
#include "hw_ioc.h"
#include "gpio.h"
#include "ioc.h"
#include "ssi.h"
#include "uart.h"
#include "sys_ctrl.h"
#include "uartstdio.h"
#include "sensor.h"
//! This example shows how to configure the SSI0 as SPI Master. The code will
//! send three characters on the master Tx then polls the receive FIFO until
//! 3 characters are received on the master Rx.
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - SSI0 peripheral
//! - GPIO Port A peripheral (for SSI0 pins)
//! - SSI0Clk - PA2
//! - SSI0Fss - PA3
//! - SSI0Rx - PA4
//! - SSI0Tx - PA5
//!
//! The following UART signals are configured only for displaying console
//! messages for this example. These are not required for operation of SSI0.
//! - UART0 peripheral
//! - GPIO Port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - None.
//
//*****************************************************************************
// --------- --|------------------
#define EXAMPLE_PIN_SSI_CLK GPIO_PIN_2
#define EXAMPLE_PIN_SSI_FSS GPIO_PIN_3
#define EXAMPLE_PIN_SSI_RX GPIO_PIN_4
#define EXAMPLE_PIN_SSI_TX GPIO_PIN_5
#define EXAMPLE_GPIO_SSI_BASE GPIO_A_BASE
#define EXAMPLE_PIN_UART_RXD GPIO_PIN_0
#define EXAMPLE_PIN_UART_TXD GPIO_PIN_1
#define EXAMPLE_GPIO_UART_BASE GPIO_A_BASE
#define ADRESS_WORD_GYRO (1 << 0)
#define ZERO_VECTOR (1 << 0)
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void
InitConsole(void)
{
//
// Map UART signals to the correct GPIO pins and configure them as
// hardware controlled.
//
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD,
IOC_MUX_OUT_SEL_UART0_TXD);
GPIOPinTypeUARTOutput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_TXD);
IOCPinConfigPeriphInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD,
IOC_UARTRXD_UART0);
GPIOPinTypeUARTInput(EXAMPLE_GPIO_UART_BASE, EXAMPLE_PIN_UART_RXD);
//
// Initialize the UART (UART0) for console I/O.
//
UARTStdioInit(0);
}
//*****************************************************************************
//
// Configure SSI0 in master Freescale (SPI) mode. This example will send out
// 3 bytes of data, then wait for 3 bytes of data to come in. This will all be
// done using the polling method.
//
//*****************************************************************************
int
main(void)
{
// Set the clocking to run directly from the external crystal/oscillator.
// (no ext 32k osc, no internal osc)
//
SysCtrlClockSet(false, false, SYS_CTRL_SYSDIV_32MHZ);
//
// Set IO clock to the same as system clock
//
SysCtrlIOClockSet(SYS_CTRL_SYSDIV_32MHZ);
//
// Set up the serial console to use for displaying messages. This is
// just for this example program and is not needed for SSI operation.
//
InitConsole();
//
// Display the setup on the console.
//
//
// The SSI0 peripheral must be enabled for use.
//************* Step 1 ******************** P123
SysCtrlPeripheralEnable(SYS_CTRL_PERIPH_SSI0);
//
// Disable SSI function before configuring module
//
SSIDisable(SSI0_BASE);
//
// Set IO clock as SSI clock source
//
SSIClockSourceSet(SSI0_BASE, SSI_CLOCK_PIOSC);
//
// For this example SSI0 is used with PA2-PA5. The actual port and pins
// used may be different on your part, consult the data sheet for more
// information. GPIO port A needs to be enabled so these pins can be used.
// TODO: change this to whichever GPIO port you are using.
//
// Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_CLK,
IOC_MUX_OUT_SEL_SSI0_CLKOUT);
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_FSS,
IOC_MUX_OUT_SEL_SSI0_FSSOUT);
IOCPinConfigPeriphOutput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_TX,
IOC_MUX_OUT_SEL_SSI0_TXD);
IOCPinConfigPeriphInput(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_RX,
IOC_SSIRXD_SSI0);
//
// Configure the GPIO settings for the SSI pins. This function also gives
// control of these pins to the SSI hardware. Consult the data sheet to
// see which functions are allocated per pin.
// The pins are assigned as follows:
// PA5 - SSI0Tx
// PA4 - SSI0Rx
// PA3 - SSI0Fss
// PA2 - SSI0CLK
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeSSI(EXAMPLE_GPIO_SSI_BASE, EXAMPLE_PIN_SSI_CLK |
EXAMPLE_PIN_SSI_FSS | EXAMPLE_PIN_SSI_RX |
EXAMPLE_PIN_SSI_TX);
//
// Configure SSI module to Motorola/Freescale SPI mode 1:
// Polarity = 0, SCK steady state is high
// Phase = 0, Data changed on first and captured on second clock edge
// Word size = 16 bits
//
SSIConfigSetExpClk(SSI0_BASE, SysCtrlIOClockGet(), SSI_FRF_MOTO_MODE_0,
SSI_MODE_MASTER, 115200, 8);
//
// Enable the SSI0 module.
//
SSIEnable(SSI0_BASE);
//
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
UARTprintf("****************OUTPUT**************\n");
while(1){
SSIDataPut (SSI0_BASE, ADRESS_WORD_GYRO);
SSIDataPut (SSI0_BASE, 0x0001);
SSIDataGet (SSI0_BASE, &i);
UARTprintf(" RECEIVE",&i);
SSIDataPut (SSI0_BASE, ADRESS_WORD_GYRO);
SSIDataGet (SSI0_BASE, &i);
UARTprintf(" HI\n\n",&i);
//
// Display indication that the SSI is transmitting data.
//
//UARTprintf("Sent:\n ",*(uint32_t*) pui32Data);
}
}