LM4F232 adc 外部参考电压 咨询

大家好,

        我使用的是TI官方的EK-LM4F232H5QD评估板,遇到了以下两个问题。

       1、其中PD4(AIN7)外接电池进行AD采样测试,电池电压1.528-1.533V左右,当设置参考电压为内部参考电压时,采样值在1827-1924,1.528/3.3*4096=1896左右,设置为外部3V参考电压时,采样值还是和内部参考电压值时差不多?为什么不是1.528/3*4096=2086左右呢?还是我的代码有问题呢(用的官方ADC例程)?更换为外部3V参考电压仅增加了红色区域的代码。请问要如何使用外部3V参考电压呢?

       2、12bit的adc,在参考电压与测试电压值都在较稳定的情况下,为什么AD采样值变化如此大?采用硬件多次平均,效果也不是特别好。

unsigned long ref=0xff;
int main(void)
{
    tContext sContext;
    char cText[8];
    unsigned long ulText;
    unsigned long ulADC0_Value[3];

    FPUEnable();
 FPULazyStackingEnable();

SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |          SYSCTL_OSC_MAIN);

    CFAL96x64x16Init();

    GrContextInit(&sContext, &g_sCFAL96x64x16);
    GrContextForegroundSet(&sContext, ClrWhite);

    GrContextFontSet(&sContext, &g_sFontFixed6x8);
 GrStringDraw(&sContext,"ADC Hands On Lab", -1,1, 5, 0);
 GrStringDraw(&sContext,"----------------", -1,1, 15, 0);
 GrStringDraw(&sContext,"Ad:", -1,20, 25, 0);

   SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);

   SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);

    GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6);

 ref=ADCReferenceGet(ADC0_BASE);
  ADCReferenceSet(ADC0_BASE,ADC_REF_EXT_3V);
 ref=ADCReferenceGet(ADC0_BASE);

    ADCSequenceConfigure(ADC0_BASE, SEQUENCER, ADC_TRIGGER_PROCESSOR, 0);

  ADCSequenceStepConfigure(ADC0_BASE, SEQUENCER, 0, ADC_CTL_CH7 | ADC_CTL_IE
                      |ADC_CTL_END);

    ADCSequenceEnable(ADC0_BASE, SEQUENCER);

    ADCIntClear(ADC0_BASE, SEQUENCER);

    while(1)
    {
        ADCProcessorTrigger(ADC0_BASE, SEQUENCER);

        while(!ADCIntStatus(ADC0_BASE, SEQUENCER, false))
        {
        }

        ADCSequenceDataGet(ADC0_BASE, SEQUENCER, ulADC0_Value);

        usprintf(cText, " %d    ", ulADC0_Value[0]);
        GrStringDraw(&sContext, cText, -1, 45, 25, 1);

        SysCtlDelay(SysCtlClockGet() / 12);

     GrFlush(&sContext);
    }
}

 

  • 楼主请参考:

    A1样片中有个Bug,配置外部参考无效的,需要置PB6的AMSEL寄存器。以后的版本会解决这个问题

    楼主可以加一句:

    HWREG(GPIO_PORTB_BASE + GPIO_O_AFSEL) |= (1 << 6);

    记得包含driverlib\gpio.h和inc\hw_gpio.h文件