如何配置SSI的位速率的相关问题(LM4F230H5QR)

用SSI读写EEPROM(25LC1024)芯片

用的是LM4F230H5QR芯片设置为主机模式,

设置1:

SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |  SYSCTL_XTAL_12MHZ);//系统时钟设置为12M

 SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 10000000, 8);//ssi位速率设置为1M

按照上面这个设设置1能够正确读写eeprom里面的数据但是如果改成下面的设置2就不行了,完全没法读数据,收数据的数组全是0,

设置2:
  

 SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL |SYSCTL_OSC_MAIN | SYSCTL_XTAL_12MHZ);// 设置系统时钟为80MHz    

 SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 10000000, 8);//ssi位速率设置为1M

 按照设置2的话,当我把位速率也就是上面的1M改成8M的时候读出来的数据就不对了,虽然能读出来但是不是我写进去的数据,  

想请教下给位,我如果系统时钟就设置成80M那么SSI的位速率应该设置成多少,或者怎么配置,麻烦给位给一个在80M系统时钟的情况下的ssi能够读写配置?

还有个问题就是我本来想看看12M的时候系统时钟配置的情况下CPSDVSR , SCR这两个参数所在寄存器的值,从而按照这个值算出80M的时候的ssi位速率应该是多的,但是ccs这个软件看不到这两个寄存器的值,怎么回事,显示的是没法读寄存器的值,

   


#include "inc/lm4f232h5qd.h"
#include "inc/hw_types.h"
#include "inc/hw_ssi.h"
#include "inc/hw_gpio.h"
#include "inc/hw_memmap.h"
#include "driverlib/ssi.h"
#include "driverlib/fpu.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/pin_map.h"
#include "driverlib/gpio.h"
#include "grlib/grlib.h"
#include "utils/uartstdio.h"

#define Uint8  unsigned char
unsigned long x;
// Number of bytes to send and receive.

#define NUM_SSI_DATA  3
unsigned char ulDataTx[NUM_SSI_DATA]={0Xfa,0Xbf,0Xcc};
unsigned long ulDataRx[NUM_SSI_DATA];

 


#define WRITECODE   0x02
#define READCODE    0x03
#define WREN        0x06
#define WRDI        0x04
#define SPI_ADD     0x0000ff
#define SE 0xd8

#ifdef DEBUG
void
__error__(char *pcFilename, unsigned long ulLine)
{
}
#endif
///////////////////////////////////////////////////////////////////////////////
unsigned char Get_Byte(void)   //接收字节
{
 unsigned long ReadData;
 SSIDataPut(SSI1_BASE, 0xFF);   //  发送一个无效字节,以产生接收时钟
 SSIDataGet(SSI1_BASE, &ReadData);
 return (unsigned char)ReadData;
}
void Send_Byte(unsigned char data)  //发送字节
{
 unsigned long NullData;
 SSIDataPut(SSI1_BASE, data);
 SSIDataGet(SSI1_BASE, &NullData);
}
void delay (unsigned long uld)   //延时
{
  for( ;uld ;uld--);
}
void  SSI_WRITE_ENABLE(void)   //写使能
{
 //SPROM_CSL=0;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);
 SSIDataPut(SSI1_BASE, WREN);
 delay (10);
 //SPROM_CSL=1;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);
}
void  SPI_WRITE_DISABLE(void)   //写禁止
{
    //SPROM_CSL=0;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);
 SSIDataPut(SSI1_BASE, WRDI);
 delay (10);
 // SPROM_CSL=1;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);
}
void SPI_CLEAR(unsigned long SPI_WRITE_ADD)
{
//    SPROM_CSL=0;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);

 SSIDataPut(SSI1_BASE, SE);   //页清除命令
 SSIDataPut(SSI1_BASE, ((SPI_WRITE_ADD & 0xFF0000) >> 16));
 SSIDataPut(SSI1_BASE, ((SPI_WRITE_ADD & 0x00FF00) >> 8));
 SSIDataPut(SSI1_BASE, ((SPI_WRITE_ADD & 0x0000FF) >> 0));
 delay (50);
//    SPROM_CSL=1;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);
}

///////////////////SSI写数据/////////////////////////////////
void SSI_WRITE(unsigned long SSI_WRITE_ADD ,unsigned char SSI_WRITE_DATA)
{

 while(SSIBusy(SSI1_BASE)){}
 //delay (10000);
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);//SPROM_CSL=0;
 //发送写的命令
 SSIDataPut(SSI1_BASE, WRITECODE);
 //写地址
 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0xFF0000) >> 16));
 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0x00FF00) >> 8));
 SSIDataPut(SSI1_BASE, (Uint8)(SSI_WRITE_ADD & 0x0000FF));

 SSIDataPut(SSI1_BASE, SSI_WRITE_DATA);
 while(SSIBusy(SSI1_BASE)){}//等待数据发送完成

 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);//SPROM_CSL=1;

}
void SSI_WRITE_NBYTE(unsigned long SSI_WRITE_ADD ,unsigned char *SSI_WRITE_DATA,unsigned char DATA_NUM)
{
 int i;
 while(SSIBusy(SSI1_BASE)){}
 //delay (10000);
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);//SPROM_CSL=0;
 //发送写的命令
 SSIDataPut(SSI1_BASE, WRITECODE);
 //写地址
 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0xFF0000) >> 16));
 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0x00FF00) >> 8));
 SSIDataPut(SSI1_BASE, (Uint8)(SSI_WRITE_ADD & 0x0000FF));
 for (i = 0; i < DATA_NUM; i++)
 {
  SSIDataPut(SSI1_BASE, SSI_WRITE_DATA[i]);
  while(SSIBusy(SSI1_BASE)){}//等待数据发送完成
 }
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);//SPROM_CSL=1;

}
///////////////////SSI读数据/////////////////////////////////
void SSI_READ(unsigned long SSI_WRITE_ADD,unsigned long *ReadData)
{
 unsigned long temp;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);

 SSIDataPut(SSI1_BASE, READCODE);

 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0xFF0000) >> 16));
 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0x00FF00) >> 8));
 SSIDataPut(SSI1_BASE, (Uint8)(SSI_WRITE_ADD  & 0x0000FF));

 while(SSIBusy(SSI1_BASE)){}//!!!

 while(HWREG(SSI1_BASE + SSI_O_SR) & SSI_SR_RNE)//重要!!!
 {
  temp = 0x00FF & SSI1_DR_R ;
 }
 SSIDataPut(SSI1_BASE, 0xFF);   //重要!!!  发送一个无效字节,以产生接收时钟

 while(SSIBusy(SSI1_BASE)){}//!!!
 SSIDataGetNonBlocking(SSI1_BASE, ReadData);

 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);
 //return ReadData;
}
void SSI_READ_NBYTE(unsigned long SSI_WRITE_ADD,unsigned long *ReadData,unsigned char DATA_NUM )
{
 int i;
 unsigned long temp;
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,~GPIO_PIN_3);

 SSIDataPut(SSI1_BASE, READCODE);

 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0xFF0000) >> 16));
 SSIDataPut(SSI1_BASE, (Uint8)((SSI_WRITE_ADD & 0x00FF00) >> 8));
 SSIDataPut(SSI1_BASE, (Uint8)(SSI_WRITE_ADD  & 0x0000FF));
 for (i = 0; i < DATA_NUM; i++)
 {
  while(SSIBusy(SSI1_BASE)){}//!!!

  while(HWREG(SSI1_BASE + SSI_O_SR) & SSI_SR_RNE)//重要!!!
  {
  temp = 0x00FF & SSI1_DR_R ;
  }
  SSIDataPut(SSI1_BASE, 0xFF);   //重要!!!  发送一个无效字节,以产生接收时钟

  while(SSIBusy(SSI1_BASE)){}//!!!
  SSIDataGetNonBlocking(SSI1_BASE, ReadData++);
 }
 GPIOPinWrite(GPIO_PORTF_BASE ,GPIO_PIN_3,GPIO_PIN_3);
 //return ReadData;
}
///////////////////SSI初始化/////////////////////////////////
void SSI_init(void)
{
    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1); //为SSI提供时钟
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);//为GPIOF端口提供时钟

    SSIDisable(SSI1_BASE);

    //  设置SPI为主机模式0,8位数据宽度,1M的波特率//
    SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(),
                 SSI_FRF_MOTO_MODE_0,SSI_MODE_MASTER, 10000000, 8);

 GPIOPinConfigure(GPIO_PF3_SSI1FSS);//SSI功能复用配置
 GPIOPinConfigure(GPIO_PF2_SSI1CLK);
 GPIOPinConfigure(GPIO_PF1_SSI1TX);
 GPIOPinConfigure(GPIO_PF0_SSI1RX);
    GPIOPinTypeSSI(GPIO_PORTF_BASE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);

    SSIEnable(SSI1_BASE);

 //  配置片选管脚为输出
    GPIODirModeSet(GPIO_PORTF_BASE,GPIO_PIN_3, GPIO_DIR_MODE_OUT);
    GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_3,GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD);
}


// The interrupt handler for the hardware SSI
void SSI1IntHandler(void)
{
 unsigned long ulInts;
 //Read the asserted interrupt sources
 ulInts = SSIIntStatus(SSI1_BASE, true);
 // Clear the asserted interrupt sources
 SSIIntClear(SSI1_BASE, ulInts);
}

void main(void)
{

 //SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |
                 //      SYSCTL_XTAL_12MHZ);
 SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL |
     SYSCTL_OSC_MAIN | SYSCTL_XTAL_12MHZ);// 设置系统时钟为80MHz

  x=SysCtlClockGet();
    unsigned long ulindex =2;

    SSI_init();

    while(1)
 {

 SSI_WRITE_ENABLE();
 SSI_WRITE_NBYTE(ulindex,ulDataTx,3);

    delay (10000);

 SSI_READ_NBYTE(ulindex,ulDataRx,3);


 }


}

        

  • 系统时钟或 PIOSC 可用作 SSInClk 的源。当 SSI 时钟配置 (SSICC) 寄存器的 CS 域配置
    0x5时,PIOSC被选为源。在主机模式下,系统时钟或 PIOSC的速度必须至少是 SSInClk
    的两倍,而 SSInClk 不能超过 25 MHz。在从机模式下,系统时钟或 PIOSC 的速度必须至
    少是 SSIClk 12 倍,而 SSInClk 不能超过 6.67 MHz


    上面是手册中的话,很明显,你的8MHZ的频率太高了。

  • CPSDVSR , SCR这两个寄存器的值是可读的,如果无法CCS直接查看,建议用串口打印看看。