Other Parts Discussed in Thread: TM4C123GH6PM
尊敬的TI工程师:
TM4C123GH6PM如何进行flash的读写呢?API在哪里?
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/flash.h"
int main(void)
{
uint32_t pui32Data[2];
uint32_t pui32Read[2];
pui32Data[0] = 0x12345678;
pui32Data[1] = 0x56789abc;
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x00);
SysCtlDelay(20000000);
// Flash
// Erase a block of the flash.
FlashErase(0x10000);
// Program some data into the newly erased block of the flash.
FlashProgram(pui32Data, 0x10000, sizeof(pui32Data));
// Turn on red LED to indicate completion
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x02);
SysCtlDelay(20000000);
while(1)
{
}
}