This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FPD Link3应用



应用:主板支持HDMI,显示器有两种(MIPI及HDMI),主板和显示器距离12米左右,需要通过FPD Link技术提高传输距离;
问题1:是否只有HDMI(主板)转FPD Link,然后FPD Link转MIPI(显示)这种方法可操作?

问题2:如果问题1属实,那么针对主板这端,是否可以将主板接口的HDMI直接连接到DS90UH949-Q1的HDMI即可?

问题3:如果问题1属实,那么针对显示端,是否可以将显示接口的MIPI直接连接到DS90UH940-Q1的MIPI即可?是否需要额外的处理器进行处理和控制?[重要]