This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ads8513采样结果的疑问



各位TI论坛里的大佬你们好:

        我这里有一个关于ad采样结果的问题,具体来说,按照手册上的描述,当我采样范围为±10V时我得到的结果应该是下面这个样子的:

----------------------------------
LSB: 152uV
+Full-scale: 9.999848V -> 7FFF
Midscale: 0V -> 0000
One LSB below midscale: -0.000002 -> FFFF
-Full-scale: -10V -> 8000
----------------------------------

但是在实际电路中,我测到的结果如下:

----------------------------------
LSB: 152uV
+Full-scale: 9.999848V -> FFFF
Midscale: 0V -> 0000
One LSB below midscale: -0.000002 -> FFFF
-Full-scale: -10V -> 0000
----------------------------------

十分奇怪,请问是哪里配置出了问题吗?

十分感谢各位的指教!