This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS中使用for循环单步执行与全速执行的区别



最近在做dsp通过68013与pc机进行数据通信的项目!遇到一个很奇怪的问题,跟各位请教一下。 首先我采用的是68013的异步slave fifo的模式。使用BULK传输。fifo缓冲区设定大小为512*4,固件程序中自动处理数据包的长度为512. 68013的异步slave fifo传输模式的逻辑控制是用cpld和dsp共同控制的,cpld中控制读写信号,控制输出使能信号SLOE,控制片选信号CS;DSP程序中控制地址FIFO_ADR0/ADR1,并读取FIFO_FLAGB/FIFO_FLAGC标志位。整个逻辑控制都实现好了!通信也正常,数据收发都很正常。 但是在测试68013通信速度时,出现了问题!我用ccs中profile->clock->view时钟周期计算时间,然后根据发送的字节数计算速度。 现在我就发送512字节,用for循环赋值。 void Dsp_PC(char* buf,int len) { int i,k; if(0==GPIO_Input_Read(pin_FLAGB)) { while(1) { if(1==GPIO_Input_Read(pin_FLAGB)) { break; } } } if(1==GPIO_Input_Read(pin_FLAGB)) { GPIO_Output_Config(pin_ADR1,1); GPIO_Output_Config(pin_ADR0,0); for(i=0;i设置断点 *(unsigned char*)USB_68013CS=buf[i]; } } return ; } main() { 、、、、、一系列的初始化、、、 -->设置断点 asm(" NOP "); for(i=0;i<1;i++) --="">设置断点 Dsp_PC(buf,512); //buf是我自己定义的一个数据,里面存放我发送的数据,512是发送的字节数 } -->设置断点 asm(" NOP "); } 现在如果在我标注的地方设置断点,那么就是单步执行Dsp_PC中发送的数据,在全部发送完512字节后,用的时钟周期是12000左右,但是如果我只在main函数中的两个空语句asm(" NOP ");处加断点,那么是for循环自行发送512字节,这时的时钟周期是370000,两者差别30倍左右! 请教各位。谁知道这问题在哪???首先这两种方法外部因素全部一样 。 在线等、、