It works to transfer the data of SD16 channel 0 using DMA, but no matter how hard I try, it doesn't work on channel 1. I'd like to ask if there are any reference examples?
Which DMA transfer mode are you using? Do you have the correct size for the grabbing the memory. Can you confirm the memory location for the SD16 Channel 1 which you're using it should be only 2h from the Channel0.