Other Parts Discussed in Thread: MSP430G2553
昨天写了一个ADC转换的问题,通过A0通道采样。把P1.0设置为输入,但ADC10CTL0 |= ADC10SC;这条语句一执行。P1.0就有电压了,本来应该是0伏特。如果把那条语句屏蔽了,P1.0就是0V。程序代码如下:
#include <msp430g2553.h>
#define uint unsigned int
#define uchar unsigned char
#define Num_of_Results 32
static uint results[Num_of_Results]
; /*宏定义各端口,RS(CS)串行通信片选,SID(R/W)串行数据口,SCLK(E)串行同步时钟信号*/
#define RS_0 P2OUT &= ~BIT0 //RS = 0
#define RS_1 P2OUT |= BIT0 //RS = 1
#define SID_0 P2OUT &= ~BIT1 //SID = 0
#define SID_1 P2OUT |= BIT1 //SID = 1
#define SCLK_0 P2OUT &= ~BIT2 //SCLK = 0
#define SCLK_1 P2OUT |= BIT2 //SCLK = 1
uchar m;
unsigned long temp, IntDegF, IntDeg;
void ADC10_init()
{
ADC10CTL0 &= ~ENC;
ADC10CTL0 = ADC10IE+ADC10ON+ADC10SHT_2+MSC+SREF_2; //ADC10ON开启10ADC
ADC10CTL1 = CONSEQ_2+INCH_0
; ADC10AE0 |= 0X03;
ADC10SA = 0X200;
__delay_cycles(30000);
ADC10CTL0 |= ENC;
ADC10CTL0 |= ADC10SC;
ADC10CTL0 &= ~ADC10IFG;
_EINT();
//LPM0;
}
/*--------------------------------------------
delay_1ms(): 延时函数
输入参数:无
编写日期:20140722
---------------------------------------------*/
void delay_1ms()
{
uint k;
for(k=0; k<195; k++);
}
/*--------------------------------------------
delay(uint n): 延时函数,延时大约1ms
输入参数:n 延时nms
编写日期:20140722
---------------------------------------------*/
void delay1ms(uint n)
{ uint j; for(j=0; j<n; j++) delay_1ms(); }
/*写指令函数*/
void write_cmd(uchar cmd) { uchar j; j = 0xF8; RS_1; //RS=1 SCLK_0; //SCLK=0(E) for(m=0; m<8; m++) { if(j&0x80) //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0 SID_1; //SID(RW) else SID_0; //最高位不为1,写0 SCLK_0; //让SCLK产生下降沿,使液晶采样 delay1ms(1); SCLK_1; //将SCLK拉高,为一位数据采样做准备 j=j<<1; //因为先发送高位,所以每次向左移动一位 } j = cmd; j &= 0xF0; for(m=0; m<8; m++) { if(j&0x80) //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0 SID_1; else SID_0; //最高位不为1,写0 SCLK_0; //让SCLK产生下降沿,使液晶采样 delay1ms(1); SCLK_1; //将SCLK拉高,为一位数据采样做准备 j=j<<1; //因为先发送高位,所以每次向左移动一位 } j = cmd; j <<= 4; for(m=0; m<8; m++) { if(j&0x80) //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0 SID_1; else SID_0; //最高位不为1,写0 SCLK_0; //让SCLK产生下降沿,使液晶采样 delay1ms(1); SCLK_1; //将SCLK拉高,为一位数据采样做准备 j=j<<1; //因为先发送高位,所以每次向左移动一位 } RS_0; delay1ms(5); }
/*写显示数据函数*/ void write_data(uchar dat) { uchar j; j = 0xFA; RS_1; for(m=0; m<8; m++) { if(j&0x80) //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0 SID_1; else SID_0; //最高位不为1,写0 SCLK_0; //让SCLK产生下降沿,使液晶采样 delay1ms(1); SCLK_1; //将SCLK拉高,为一位数据采样做准备 j=j<<1; //因为先发送高位,所以每次向左移动一位 } j = dat; j &= 0xF0; for(m=0; m<8; m++) { if(j&0x80) //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0 SID_1; else SID_0; //最高位不为1,写0 SCLK_0; //让SCLK产生下降沿,使液晶采样 delay1ms(1); SCLK_1; //将SCLK拉高,为一位数据采样做准备 j=j<<1; //因为先发送高位,所以每次向左移动一位 } j = dat; j <<= 4; for(m=0; m<8; m++) { if(j&0x80) //判断最高位是否是为1,如果是则给SDIN赋1即写入1,否则写0 SID_1; else SID_0; //最高位不为1,写0 SCLK_0; //让SCLK产生下降沿,使液晶采样 delay1ms(1); SCLK_1; //将SCLK拉高,为一位数据采样做准备 j=j<<1; //因为先发送高位,所以每次向左移动一位 } RS_0; delay1ms(5); }
/*设定显示位置*/ void lcd_pos(uchar X, uchar Y) { uchar pos; if(X == 0) X = 0x80; else if(X == 1) X = 0X90; else if(X == 2) X = 0X88; else if(X == 3) X = 0X98; pos = X+Y; write_cmd(pos); //显示地址 }
/*LCD初始化设定*/ void lcd_init() { //P1OUT &= ~BIT3; //PSB = 1;并口方式 write_cmd(0x30); //基本指令操作 delay1ms(5); write_cmd(0x0c); //显示开,关光标 delay1ms(5); write_cmd(0x01); //清除LCD的显示类容 delay1ms(5); }
/*-------------------------------------------- Init_Port(): MSP430G2553端口初始化函数 输入参数:无 编写日期:20140722 ---------------------------------------------*/ void Init_Port() { P1DIR = 0; //将P1口所有的管脚在初始化的时候设置为输入方式 P2DIR = 0; //将P2口所有的管脚在初始化的时候设置为输入方式 //P1REN |= BIT0; //P1OUT &= ~BIT0; P1SEL |= BIT0; //将P1口所有的管脚设置为一般I/O口 P1DIR &= ~BIT0; P1DIR |= BIT4; P2SEL = 0X00; P2IE = 0X00; P2DIR = 0XFF; //将P2口所有的管脚在初始化的时候设置为输入方式 }
void display(long date) { uchar ge, shi, bai, qian; qian=date/1000; bai=date%1000/100; shi=date%1000%100/10; ge=date%1000%100%10; lcd_pos(0,2); write_data(0x30+qian); write_data(0x30+bai); lcd_pos(0,3); write_data(0x30+shi); write_data(0x30+ge); }
void main() { WDTCTL = WDTPW + WDTHOLD; BCSCTL1 = CALBC1_8MHZ; DCOCTL = CALDCO_8MHZ; Init_Port(); lcd_init(); ADC10_init(); while(1); }
#pragma vector = ADC10_VECTOR __interrupt void ADC10ISR() { uchar i; P1DIR |= BIT4; P2DIR |= BIT0+BIT1+BIT2; static uint index = 0; results[index++] = ADC10MEM; if(index >= Num_of_Results) { unsigned long sum = 0;
index = 0; for(i = 0; i < Num_of_Results; i++) { sum += results[i]; } sum >>= 5; //除以32 temp = 3300*sum/1023; display(temp); } }