Other Parts Discussed in Thread: TPA3255-Q1, , TPA3116D2-Q1, TPA3255
Please help check the following question:
1. TPA3116-Q1 Juntion temp is -40~150degC?
2. TPA3255-Q1 Junction temp is -40~125degC?
3. TPA3223 Juntion temp is 0~125degC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please help check the following question:
1. TPA3116-Q1 Juntion temp is -40~150degC?
2. TPA3255-Q1 Junction temp is -40~125degC?
3. TPA3223 Juntion temp is 0~125degC?
Hi,
You can confirm the temp in datasheet.
1,I couldn't find the TPA3116-Q1. If you meant to check the junction temperature of the TPA3116D2-Q1?
For TPA3116D2-Q1
Absolute Maximum Ratings
Operating junction temperature range, TJ :–40 to 150 °C
www.ti.com/.../tpa3116d2-q1.pdf
2, TPA3255-Q1
Recommended Operating Conditions
TJ Junction temperature :-40 to 125 °C
3, TPA3223
Recommended Operating Conditions
TJ Junction temperature :0 to 125 °C
Hi wenjie,
For all of the device max temperature, please all use OTSD value as max supported junction temperature.
TPA3223 seems not an automotive part, may not fully support to -40C working.
Hi
As I check this device's design target still take -40C as minimum working range.
But it's already not our group's device, let me transfer to other team, to see if they have any further commence.
this should be a typo miss in DS. -40degree should be the correct value.