This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
德仪的很多音频 CODEC 芯片, 控制简单, 只需要有 i2c 或者 SPI 接口就可以控制
可以去这里找 http://www.ti.com.cn/lsds/ti_zh/audio-ic/audio-codec-product.page
你好,
主要是想用MSP430完成CODEC的数据采集及搬运(给FPGA),430不做音频信号处理。我现在用的是MSP430F5438A,CODEC型号是TLV320AIC14k,采样率要求是8k,16bit,不知道是否可行?或者有没有其它的办法?(最好还是用430)
此外,TLV320AIC14k的串行接口是SMART TDM(TI有不少这样接口的CODEC)。SMART TDM接口有FSD/DOUT/DIN/FS/SCLK五线,其中FSD用于设置主从模式,其它四线跟SPI协议很像。想问的是,SMART TDM是否跟SPI接口兼容?
谢谢!
晚上看了下手册:
MSP430F5438A的SPI只支持7位或8位数据宽度,而TLV320AIC14K是一款16位的CODEC,时序上也略微不一样,SMARTTDM是带有帧同步信号的。
头疼了,这种情况下5438A的SPI还能与TLV320AIC14K的SMARTTDM连接吗?有什么高招吗
貌似MSP430 没有Mcbsp接口?
TI低端的处理器可以跟CODEC芯片进行数据交互的,只有C55X系列?
MSP430没有这个接口。其它的带I2S只有ARM系列的MCU和C5000、6000 DSP,具体可以到处理器的板块问问。