TAC5112: Generate a sine wave using the TAC5112

Part Number: TAC5112


I attempted to use the TAC5112 to output a sine wave but found that the actual tested waveform was not perfect. Upon reviewing the chip datasheet, I noticed that the device itself supports a signal generation function. Therefore, I tried using this feature to make the OUT1P pin output a sine wave. After referring to the application manual(Tone Generation and Application Modes of TAx5x1x Devices ), I performed the following I2C configuration without making any other additional settings or operations, but no output was observed. 
tac_cfg_reg_t tac_registers[] = {
// #define CHECKSUM (0)
    {0x00,0x00},//  locate page x00 
    {0x01,0x01},//  device reset 
    {0x00,0x00},//  locate page x00 
    {0x02,0x09},//  vref and dreg enable 
    {0x00,0x01},//  locate page x01 
    {0x2d,0x08},//  enable SG1
    // Channel selection and amplitude configuration
    {0x00,0x11}, //  locate page 0x11 
    {0x68,0x40}, 
    {0x69,0x00},
    {0x6a,0x40}, 
    {0x6b,0x00}, //  mix SG1 to DAC1 L & R Channels and
                        //  set the amplitude to full-scale, 0dB. 
    // Frequency configuration 
    {0x00,0x00}, //  locate page 0x00 
    {0x7f,0x00}, //  locate book 0x00 
    {0x00,0x12}, //  locate page 0x12 
    // 600Hz 
    {0x20,0x99}, 
    {0x21,0x7f},
    {0x22,0xec}, 
    {0x23,0x00}, 
    {0x24,0x7f}, 
    {0x25,0x9a}, 
    {0x26,0xfc}, 
    {0x27,0xb8}, // sinx and cosx upper bits 

    {0x28,0x1c}, 
    {0x29,0xea}, 
    {0x2a,0xf1}, 
    {0x2b,0x80}, 
    {0x2c,0x0a}, 
    {0x2d,0x0a}, 
    {0x2e,0xf2}, 
    {0x2f,0x99}, // sinx and cosx lower bits 
    // Output configuration 
    {0x00,0x00}, //  locate page 0x00 
    // differential mode is the default output mode 
    {0x64,0x24},// option to set to single-ended mode 
    // {0x64,0x28},//关闭ADC HPF滤波器
    // {0x6b,0x00},//关闭ADC HPF滤波器
    // {0x72,0x00},//关闭ADC HPF滤波器
    {0x76,0x0c}, // enable DAC1, CH 1 & 2 180deg out of phase diff. mode 
    {0x78,0x40}, // enable DAC
};