Other Parts Discussed in Thread: UAF42
如题,输入信号频率500kHz,幅值1-10V,由于信号易受干扰需要尽可能低噪声的陷波器,请问有推荐的芯片和陷波器结构吗,谢谢
这个没有现成的设计或者产品,下面的资料都是相关的,可以参考:
Dear TI engineers:
I would like to design a low-noise 50Hz notch filter. The first requirement is that its PSD noise should be sufficiently low: 1uV/rt(Hz) at 1Hz, 10nV/rt(Hz) at 10KHz. Then its power consumption should be less than or equal to 10mA. I would like to ask if this can be achieved at the analog end? We have tried the basic UAF42, dual T, and Fliege, but none of them meet our requirements. It is still recommended that I can only achieve it through digital filtering methods.
对于您的具体要求,我们没有实际的设计可供参考。
建议合理选择运算放大器和电阻值,注意元件容差、温度稳定性以保持陷波深度,并通过仿真验证噪声性能。