This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAA5212: Does the following information indicate that the ADC of the TAA5212 chip can be configured as 16-bit, 20-bit, 24-bit, or 32-bit?

Part Number: TAA5212

This information is derived from the TAA5212 datasheet:

By using the PASI_FORMAT[1:0] (P0_R26_D[7:6]) register bits, the bus protocol TDM, I2S, or Left Balanced (LJ) format can be selected for the primary ASI. As shown in Tables 6-2 and 6-3, these modes are all Pulse Code Modulation (PCM) data formats with the most significant byte (MSB) taking precedence. The output channel data word length can be programmed to 16, 20, 24, or 32 bits by configuring the PASI_WLEN[1:0] (P0_R26_D[5:4]) register bits.