我的板子上的时钟源是24MHz的晶振。
1. 从pcm1864手册上看到,reg32(0x20)寄存器配置时钟源选择,选择XTAL作为时钟源,主模式,clkdet enable,写入值0x11,读出值0x17,寄存器值是否正常?
2. 在1的基础上,使能pll_en。
3. 查看reg117(0x75),值为0x7,几项时钟都出错,请问我该怎么解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的板子上的时钟源是24MHz的晶振。
1. 从pcm1864手册上看到,reg32(0x20)寄存器配置时钟源选择,选择XTAL作为时钟源,主模式,clkdet enable,写入值0x11,读出值0x17,寄存器值是否正常?
2. 在1的基础上,使能pll_en。
3. 查看reg117(0x75),值为0x7,几项时钟都出错,请问我该怎么解决?
读写寄存器值不一样,显然是不正常的,除了24MHz的crystal输入之外,MCK多大频率?LRCK,BCK是外部时钟提供还是通过内部分频得到?
感谢您的回答,我修改了外部晶振为8MHz,master模式,PLL disable, DSP1/DSP2/ADC时钟采用SCK(即外部晶振时钟),这样是可以工作了, LRCK/BCK/DOUT都是有输出的,但是不确定是否正确。
目标配置为:16K采样率、4个mic、16bits采样率,两路Dout。请问按照以下这样的配置是否能满足?
工作模式: master, LRCK/BCK由pcm1864产生。
clock: SCK ----- 采用外部晶振,8MHz
DSP1 ----- 1/2 SCK (4MHz)
DSP2 ----- 1/2 SCK (4MHz)
ADC ----- 1/4 SCK (2MHz)
BCK ----- 1/8 SCK (1MHz)
LRCK ----- 1/64 SCK (125KHz)
ADC1L/ADC1R/ADC2L/ADC2R:
vin1L/vin1R/vin2L/vin2R
GPIO1: 复用为Dout2
output format: I2S
TDM: default(Dout1: CH1(L) CH1(R); DOUT2: CH2(L), DOUT2(R))