Other Parts Discussed in Thread: TAS5711
TAS5711发生PLL autolock error错误,这个错误怎么解决,急。。。。。。。。。。。。。。。。。。。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TAS5711
TAS5711发生PLL autolock error错误,这个错误怎么解决,急。。。。。。。。。。。。。。。。。。。
Hi Karmond,
你的I2S输入MCLK/BCLK/LRCLK是多少?是不是用了三根线的模式?
Hi Karmond,
TAS5711三线I2S的模式,这样的模式只支持44.1K和48K,需要将MCLK引脚连接到BCLK,且BCLK配置为64*FS,请参考TI的Wi-Ki
https://e2e.ti.com/support/amplifiers/audio_amplifiers/w/design_notes/2425.i2s-clock-requirements-on-tas570x1x2x3x-device-s
1.) For most TASS57xx devices, 44.1/48-kHz mode allows the use of a 64*Fs MCLK rate. This rate also happens to be one of the supported SCLK rates. In system's where only one clock may be available, a common MCLK=SCLK=64*Fs rate is an option to overcome the limitation. -- This is valid only if the Fs rate is 44.1/48-kHz.