Part Number: TAS5825M
TAS5825M如何将音频转换为烧录文件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
请参考数据手册34页“9.4.1 Software Control”的描述,www.ti.com.cn/.../tas5825m.pdf
There are two methods to program TAS5825M DSP memory. • Loading with I2C Communication Port by host processor. This method is recommend for most of applications. • Fast loading from external EEPROM with SPI communication Port. This method can be used in some applications which need fast loading to save initialization time or release the Host Controller's loading. TAS5825M supports to load the DSP memory data from external EEPROM via SPI. The GPIOs can be configured as SI,SO and SCK for EEPROM via Register (0x60,0x61,0x62,0x63,0x64). The chip selection CS of EEPROM is controlled by the Host Processor. See AppNote: Load TAS5825M Configurations from EEPROM via SPI.