This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
aic23b的ADC输入信号范围是多少,如何计算得出电压
请参考Datasheet里 absolute maximum rating
最大-0.3-AVDD
你好,Absolute Maximum Ratings是芯片的输入信号范围还是ADC的输入电压范围,还有数据手册上为什么说满量程是1 Vrms呢?
你好
1Vrms 对应的是2.8 Vpp,
你好,那设置16位数据时,数字量如何计算成电压呢?谢谢
Full- scale 对应满量程
您好,我对这个问题也有疑问,datasheet上这个介绍的太模糊了.想问一下AIC3106 ADC和DAC的电压范围是多少?16 bit的AD和DA 是不是意味着最大值32767和最小值-32768?那么这两个值分别对应电压是多少?非常感谢!