IT專家您們好, 請問 TPA3123 在使用 shutdown 時, 當在正常工作把 shoutdown high = operational 後, 偶爾音频會出現延遲大概 5-8秒才有輸出, 謝謝幫忙.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有没有可能是输出级挂了比较大的容性负载,在power down/on切换时,需要对较大的容性负载充放电,从而导致了较长时间的延迟?
你好!
建议监控out_21引脚对应的光耦后的引脚,将这两个信号进行对比,观察有无出现延时现象,其次,将输出信号也与out_21引脚进行时序对比,主要是为了查找出造成延时的位置点,然后可以帮助我们分析可能带来延时的因素,以进一步消除延时。
把out_21脚pull high,shutdown的电位是下面哪一种情况?

"shoutdown脚的電位需要一段時間才會尤 0V 跳上 24V的."
如你所言,如果可能的话,可以计算一下大概是多长时间,与你的说的5~6s相差多大,这样基本上可以确定是不是由于光耦带来的影响,如果是的话,那可能可以考虑更换光耦或者采用一些措施来使其变化更快。
可能这个10k电阻确实有点大,建议可以通过查看光耦的datasheet上的推荐来选择一个更合适的上拉电阻,同时建议可以直接通过示波器,查看具体带来的时延到底是多大,这样有利于定量的满足要求。