工程师们,你们好,现在我这边想通过AIC3254的静默检测的中断功能实现这样一个应用:
当MIC的signal大于噪声门限(Noise Threshold)时,我将采集音频数据,发送给终端用户,当MIC的signal小于噪声门限(Noise Threshold)时,我不再发送数据
我的具体实现方式是:
1:配置INT1中断为:INT1 Interrupt for AGC Noise Interrupt(Page 0 / Register 48);
2:将AIC3254的GPIO设置为: GPIO output is INT1(Page 0 / Register 52);
3:将此GPIO连接到MCU的GPIO,MCU检测此IO的中断,若发生中断,读取相应状态寄存器(Page 0 / Register 45:D5、D6)根据响应状态决定是否是有效音频数据并决定是否发送数据。
请问此方案是否可行?若可行,我上边配置是否正确,还需要配置其他寄存器吗?我现在这样配置中断上不来(我测了AIC3254的GPIO,无论静默还是大声说话时,都没有电平变化)。