This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5611APHDR与TAS5611APHD有什么区别?

Other Parts Discussed in Thread: TAS5611A, TAS5630

TAS5611APHDR与TAS5611APHD有什么区别?TAS5611APHDR是否可以应用到TAS5611A说明书上的电路图吗?AD mode与BD mode工作模式有什么区别?

tas5611a.pdf
  • 两个编号的IC是一样的,只是盛载IC的盘不一样。关于AD、BD mode,AD是在输出作逻辑反相产生负端输出,所以输出正负端PWM永远是反相。而BD则是在输入作模拟反相产生负端输入再输出到负端输出,特点是在无音频输入时,输出正负端PWM是同相。

  • 谢谢!再问一个问题,mode PINS设置M3,M2,M1为1,0,1,即PBTL模式,但是输入由差分输入改为单端输入,这样设置可以吗?是否会有其他隐患呢?

  • TAS5630實際上是4個獨立單端的設計,BTL只是把2個單端接在一起。M1、2、3只是對應不同的輸出保護。那就是說輸入和輸出是一一對應,那一個單端有輸入就會有輸出,沒有輸入就沒有輸出。所以如果只有單端輸入而不是差分,其中一個輸出腳便有輸出,這樣最大可達到的最大功率就會變得很小,只有BTL最大輸出功率的四分之一

  • 对不起,是指TAS5611A,其实这点跟TAS5630是一样,另外用了繁体字,这是简体。TAS5611A实际上是4个独立单端的设计,BTL只是把2个单端接在一起。M1、2、3只是对应不同的输出保护。那就是说输入和输出是一一对应,那一个单端有输入就会有输出,没有输入就没有输出。所以如果只有单端输入而不是差分,其中一个输出脚便有输出,这样最大可达到的最大功率就会变得很小,只有BTL最大输出功率的四分之一。