Other Parts Discussed in Thread: TAS5766M
各位工程师:
您好,我们是用TAS5766M在基于mstar芯片做tv板,能否提供TAS5766M在linux下面的驱动?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kes,您好,
是这样,我们发现这个芯片即使不初始化也能用。但是声音效果不好,而实际上很多tv厂都用这个芯片效果很好。要不然我把问题细化一下:
1) Init的时候是否做哪些操作呢?
2) 有的声音设置有各种模式,比如人声,重低音,高保真,这些i2c怎么设置
3) 还有我们其实mstar给了5711的Init参考代码,里面有些注释,我想问一下您能否对应这个给一份5766M的,谢谢!
MAPI_BOOL device_audio_amp_I2S_TI5711::Init(void)
{
MAPI_U8 * Pstr = NULL;
MAPI_U8 DataLength = 0;
MAPI_U8 g_ucTas5711RegAddr = 0;
MAPI_U8 AmpInitBin[1024];
MAPI_U8 AmpInitTbl[] =
{
//DataLength Address DataN DataN+1...
// I2C Configuration file for TAS5700x
1, 0x1B, 0x00,
1, 0x06, 0x00,
1, 0x0A, 0xff,
1, 0x09, 0x30,
1, 0x09, 0x29,
1, 0x08, 0x29,
1, 0x14, 0x54,
1, 0x13, 0xAC,
1, 0x12, 0x54,
1, 0x11, 0xAC,
1, 0x0E, 0xD1,
1, 0x1A, 0x95,
4, 0x20, 0x00, 0x01, 0x77, 0x72,//modify data[20][16] for LR channel config
4, 0x21, 0x00, 0x00, 0x42, 0x03,
1, 0x10, 0x02,
1, 0x0B, 0x00,
1, 0x10, 0x02,
1, 0x1C, 0x02,
1, 0x19, 0x30,
4, 0x25, 0x01, 0x01, 0x32, 0x45,
// Biquads
4, 0x50, 0x00, 0x00, 0x00, 0x00,
20, 0x29,0x00,0x80,0x4F,0xD0,0xFF,0x03,0xBF,0x07,0x00,0x7C,0x61,0x5B,0x00,0xFC,0x40,0xF9,0xFF,0x83,0x4E,0xD4,
20, 0x2A,0x00,0x80,0x19,0x16,0xFF,0x04,0x16,0x3F,0x00,0x7C,0x98,0x15,0x00,0xFB,0xE9,0xC1,0xFF,0x83,0x4E,0xD4,
20, 0x2B,0x00,0x80,0x77,0x6E,0xFF,0x11,0xCD,0x6B,0x00,0x6F,0xC9,0x54,0x00,0xEE,0x32,0x95,0xFF,0x8F,0xBF,0x3D,
20, 0x2C,0x00,0x83,0xDB,0x0D,0xFF,0x2F,0x00,0x81,0x00,0x5E,0x5C,0xB7,0x00,0xD0,0xFF,0x7F,0xFF,0x9D,0xC8,0x3B,
20, 0x2D,0x00,0x85,0x7F,0xA9,0xFF,0x56,0x99,0x07,0x00,0x50,0x07,0x36,0x00,0xA9,0x66,0xF9,0xFF,0xAA,0x79,0x20,
20, 0x2E,0x00,0x85,0x7F,0xA9,0xFF,0x95,0x3C,0x90,0x00,0x50,0x07,0x36,0x00,0x6A,0xC3,0x70,0xFF,0xAA,0x79,0x20,
20, 0x2F,0x00,0x80,0x6D,0xA1,0xFF,0x03,0x69,0xA7,0x00,0x7C,0x43,0x8A,0x00,0xFC,0x96,0x59,0xFF,0x83,0x4E,0xD4,
20, 0x30,0x00,0x80,0x4F,0xD0,0xFF,0x03,0xBF,0x07,0x00,0x7C,0x61,0x5B,0x00,0xFC,0x40,0xF9,0xFF,0x83,0x4E,0xD4,
20, 0x31,0x00,0x80,0x19,0x16,0xFF,0x04,0x16,0x3F,0x00,0x7C,0x98,0x15,0x00,0xFB,0xE9,0xC1,0xFF,0x83,0x4E,0xD4,
20, 0x32,0x00,0x80,0x77,0x6E,0xFF,0x11,0xCD,0x6B,0x00,0x6F,0xC9,0x54,0x00,0xEE,0x32,0x95,0xFF,0x8F,0xBF,0x3D,
20, 0x33,0x00,0x83,0xDB,0x0D,0xFF,0x2F,0x00,0x81,0x00,0x5E,0x5C,0xB7,0x00,0xD0,0xFF,0x7F,0xFF,0x9D,0xC8,0x3B,
20, 0x34,0x00,0x85,0x7F,0xA9,0xFF,0x56,0x99,0x07,0x00,0x50,0x07,0x36,0x00,0xA9,0x66,0xF9,0xFF,0xAA,0x79,0x20,
20, 0x35,0x00,0x85,0x7F,0xA9,0xFF,0x95,0x3C,0x90,0x00,0x50,0x07,0x36,0x00,0x6A,0xC3,0x70,0xFF,0xAA,0x79,0x20,
20, 0x36,0x00,0x80,0x6D,0xA1,0xFF,0x03,0x69,0xA7,0x00,0x7C,0x43,0x8A,0x00,0xFC,0x96,0x59,0xFF,0x83,0x4E,0xD4,
20, 0x5A,0x00,0x00,0x05,0x83,0x00,0x00,0x0B,0x06,0x00,0x00,0x05,0x83,0x00,0xFB,0x42,0xC1,0x0F,0x84,0xA7,0x33,
20, 0x5B,0x00,0x00,0x05,0x83,0x00,0x00,0x0B,0x06,0x00,0x00,0x05,0x83,0x00,0xFB,0x42,0xC1,0x0F,0x84,0xA7,0x33,
// DRCs
8, 0x3A, 0x00,0x05,0x39,0x47,0x00,0x7A,0xC6,0xB8,
8, 0x3B, 0x00,0x05,0x39,0x47,0x00,0x7A,0xC6,0xB8,
8, 0x3C, 0x00,0x00,0x00,0xF9,0x00,0x7F,0xFF,0x06,
4, 0x40, 0xFD,0xA2,0x14,0x90,//0xFD,0xc1,0xf8,0x89,//0xFC, 0x83, 0x10, 0xD4, //4, 0x40, 0xFD, 0xe1, 0xdc, 0x81,//
4,0x41,0x0F,0x81,0x47,0xAF, //б
4, 0x42, 0x00, 0x08, 0x42, 0x10,
4, 0x46, 0x00, 0x00, 0x00, 0x03,
8, 0x39, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
8, 0x3D, 0x00,0x05,0x39,0x47,0x00,0x7A,0xC6,0xB8,
8, 0x3E, 0x00,0x05,0x39,0x47,0x00,0x7A,0xC6,0xB8,
8, 0x3F, 0x00,0x00,0x00,0xF9,0x00,0x7F,0xFF,0x06,
4, 0x43, 0xFD,0x82,0x30,0x98,//0xFC, 0x83, 0x10, 0xD4,
4, 0x44, 0x0F, 0x83, 0x33, 0x34,
4, 0x45, 0x00, 0x08, 0x42, 0x10,
4, 0x46, 0x00, 0x00, 0x00, 0x03,//0x03,
//12, 0x52, 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
//8, 0x60, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00,
//4, 0x56, 0x00, 0x80, 0x00, 0x00,
//4, 0x57, 0x00, 0x02, 0x00, 0x00,
//16, 0x53, 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00,
//16, 0x54, 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x80, 0x00, 0x00,
//12, 0x55, 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
//12, 0x51, 0x00, 0x80, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
1, 0x07, 0xFF,
1, 0x05, 0x84,
1,0x0D,0x35,
0x00,
};