This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA31180D2的LC网络电感值选择



1、我在使用TPA3118D2设计一个功放,要求是15V电源,4欧姆喇叭,功率在15W,BTL模式,但是在后面的LC的电感选择上出现了问题,不知道如何选择电感值的大小

2、我看其他帖子上说是根据Q值、截止频率来选择的,但是电感的参数不应该是以电流为准的吗?我还想知道输出声道上的电流如何计算的?就是下图中红色圈内的电流

我的原理图基本上按照TPA3118D2EVM设计的。谢谢各位给予解答!!!

  • 电感的参数, 电流也是一个重要参数, 特别是带磁芯的电感, 承受电流范围以外可能导致进入磁饱和的非线性区域而导致电感特性变差.

    但是这个参数却不再计算范围内. 你应该根据工作最大电流选择合适的电感.

    而这个电流, 可以通过电压和阻抗来计算