This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

音频小白,咨询下PCM1804音频输入和输出问题

Other Parts Discussed in Thread: PCM1804, PCM1793

问题:用PCM1804做音频转换,最终输出声音很难听

使用环境:用科大讯飞的TTS芯片XFS5152CE输出模拟音频到PCM1804,(TTS输出是搭载在1.5V直流上的音频信号,输出引脚串联1uF电容直连到PCM1804左声道正负引脚),PCM1804输出PCM音频直连到华为全网通模块ME909S-821mini。实测时TTS芯片输出到PCM1804引脚的音频信号很好(好听的女声),PCM1804输出到ME909S-821mini采用主模式,LRCK为16kHz,BCK为1.024mKz,测两端的信号都很好,但是通过电话接听到ME909S-821mini输出的声音很难听,而且是男声了。

目前还不确定问题在哪里,就TTS和PCM之间来检测,有几个可能,TTS输出到PCM的信号需要调制到2.5V的中心电压(已测试,无效果);TTS输出到PCM的声音信号峰值需放到2.5V。PCM和ME909S-821mini之间的问题暂时没有器件来替换查找。

希望各位大侠帮忙看看问题在哪,万分感谢

下面是PCM电路,9、10脚已拉低,因为当频率大于32kHz时,ME909S-821mini打电话会自动挂机。

TTS输出

PCM用作主模式,输出音频与ME909S-821mini直连

  • 这个问题挺奇怪的. 声音很难听, 而且女声变男声, 往往跟失真或信号断续有关.

  • 对输入PCM1804的模拟音频加2.5V的偏置电压后,对比不做处理的声音,只是稍微清晰、响亮一些,依旧是较模糊的男声。放大声音信号,对声音效果几乎没影响。在加偏置测试的时候,用的单电源运放,把声音信号下半周削去了,这个对PCM音频处理有影响,但应该不大,监测加偏置后耳机里面的声音还是质量很好的女声。

    目前准备用PCM1793把PCM1804输出的音频取出来听下效果。

    请问,有没有什么简单的方法可以得到一个PCM音频信号输给ME909s试试?

  • 我用PCM1793将PCM1804输出的音频转换到耳机,声音效果和输入PCM1804的模拟音频效果相当,现在确定音源处理阶段没问题。那应该是PCM1804和无线模块ME909s之间的传输出了问题,由于PCM1804是主模式,时钟应该没问题,两个信号电平匹配也没问题,数字信号的干扰似乎也不足以让清晰的女声变成模糊的男声,那还有哪里存在问题呢?

x 出现错误。请重试或与管理员联系。