Other Parts Discussed in Thread: PCM9211
PCM9211有个ADC Level Detect and Interrupt功能,想把它做到无信号自动待机,但是我在设定Level Detector值至-48dB时,低信号时INT1仍然无电平跳变(即PCM9211判定这时无信号输入),直至ADC输入信号电平很高时INT1才有电平跳变。请问怎样准确检测有无信号,做到无信号自动待机。请帮忙解答,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCM9211
PCM9211有个ADC Level Detect and Interrupt功能,想把它做到无信号自动待机,但是我在设定Level Detector值至-48dB时,低信号时INT1仍然无电平跳变(即PCM9211判定这时无信号输入),直至ADC输入信号电平很高时INT1才有电平跳变。请问怎样准确检测有无信号,做到无信号自动待机。请帮忙解答,谢谢!
hi Airwill
现在的问题是配置过下面几个值都不能精确的检测出输入信号是否存在?输入信号幅度很大时才能检测出,不知道哪里没有配置好?请指点
ADLVLTH[1:0]: ADC Input Level Detection Threshold for INT1
00: –12dB
01: –24dB
10: –36dB
11: –48dB