This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3104 输出有噪声求解答:

Other Parts Discussed in Thread: TLV320AIC3104

情况是这样的:
环境配置:
     将功放(漫步者R101V)输出调整到最大。
A.  将功放输入插入到台式电脑、手机等,在台式电脑或手机都没有没有播放情况下,功放输出是听不到噪声。
B. 将功放输入插入TLV320AIC3104的输出端口有如下现象:
1. 配置3104的信号通路为   I2S输入--->DAC--->HPOUT 。在I2S输入为静音(数据线始终为0)的状态下,初始化配置3104,此时3104的HP输出无噪声。当I2S输入一段音频信号,然后重新处于静音状态时,3104的输出出现噪声信号,且此噪声信号一直保持。
2. 在出现此噪声的状态下,power down DAC,并重新power upDAC,此噪声消失。但如果从I2S输入音频,此噪声又出现
3. 将3104的信号通路设置为MIC输入--->PGA---->HP输出,则不会观察到上述的噪声。
4. 设置DAC为mute(Reg43.D7=1  Reg44.D7=1),输出噪声消失,再将DAC设置为unmute,噪声依然会出现。同时调整Reg43和Reg44的增益,对输出噪声的幅值没有影响。