This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助TPA6133A2单端输入阻抗匹配的问题

Other Parts Discussed in Thread: TPA6133A2

datasheet里面关于音频输入的引脚描述如下——

LEFTINM: Left channel negative differential input. Impedance must be matched to LEFTINP. Connect the left input to LEFTINM when using single-ended inputs.

LEFTINP: Left channel positive differential input. Impedance must be matched to LEFTINM. AC ground LEFTINP near signal source while maintaining matched impedance to LEFTINM when using single-ended inputs.

我想请教一下,如果单端输入时前面是DAC+LPF(例如PCM510xA),那LEFTINP要如何交流接地同时保持阻抗匹配?PCM510xA的Load impedance: 1 kΩ(min).

PCM510xA应用图:

  • PCM510x的1Kohm的阻抗指的是负载阻抗,指的是起内部的line driver的带载能力。

    而TPA6133A2的datasheet中强调的是差分传输线的走线阻抗要匹配,防止信号发生发射。

  • 差分传输线的走线阻抗要匹配?可是这是音频,这么低频分布参数不明显,应该不考虑走线阻抗吧?不应该是考虑从运放输入端向外看的戴维南等效电阻吗?不过我觉得这样真的太复杂了,不仅有电阻,还有电容。

    我提到PCM510x的负载阻抗最小为1Kohm,主要是希望考虑其内阻,datasheet里面没有直接给出其输出阻抗。希望继续解答我的疑惑,非常感谢!