Other Parts Discussed in Thread: TAS5614
只使用A、B两个通道,C、D相关的管脚比如29 30 31管脚的PVDD-CD 22管脚的GVDD-CD;16 17管脚的 INPUT C、D ;27 28 32管脚的OUT C 、D;23 24管脚的BST-C D 这几个管脚能否直接接地呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不用的输入通道Channel C,D可通过一10uF电容到地,输出以及BST_C和BST_D可直接悬空。在TAS5614的datasheet中有对不用的channel进行描述,请参考:
If all available output channels are not used, TI recommends disabling switching of unused output nodes to reduce power consumption. Furthermore by disabling unused output channels the cost of unused output LC demodulation filters can be avoided. Disabling a channel is done by leave the bootstrap capacitor (BST) unstuffed and connecting the respective input to GND. The unused output pin(s) can be left floating.
Kailyn Chen 说:不用的输入通道Channel C,D可通过一10uF电容到地,输出以及BST_C和BST_D可直接悬空。在TAS5614的datasheet中有对不用的channel进行描述,请参考:
If all available output channels are not used, TI recommends disabling switching of unused output nodes to reduce power consumption. Furthermore by disabling unused output channels the cost of unused output LC demodulation filters can be avoided. Disabling a channel is done by leave the bootstrap capacitor (BST) unstuffed and connecting the respective input to GND. The unused output pin(s) can be left floating.
谢谢你 还想请教下 GVDD_CD和PVDD_CD 也可以接电容接地么 还是需要接到电源