最近需要用到咪头采集人体的生理信号,咪头的灵敏度在-34dB以上,信噪比大于58dB,频率响应范围在20Hz到16000Hz。不过昨天我将咪头的两个引脚接入OPA1612放大电路没有任何信号,想问一下咪头采集电路是怎样的?另外由于后期要进行放大和滤波,滤波后再20Hz到1500Hz,想问一下除了OPA1612芯片,是否还有更好的推荐?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
咪头采集的话,可以考虑LMV1012,LMV1032.
除了OPA1612的话,还可以看下OPA2134。