Other Parts Discussed in Thread: PCM1808
您好,这里AD转换器与SPI接口之间是怎样通讯的,数据传输是怎样的,一个是16位的,一个是24位的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCM1808
您好,这里AD转换器与SPI接口之间是怎样通讯的,数据传输是怎样的,一个是16位的,一个是24位的
PCM1808是怎样使用的,现在要做的是用它采集数据,将它传到DSP的RAM上,最后是通过串口再传到上位机上面,然后进行分析,不知道PCM1808是怎样进行编程的,希望给予解答,谢谢!我的邮箱是 812515899@qq.com
PCM1808是音频的ADC, 不是普通的ADC,使用I2S接口,请确认您是需要该种音频ADC
您好,那如果是普通的ADC的编程是怎样的呢,如果是24位的数据的话
初学这个,好多东西都不明白,现在要做的是假如已经采好了数据,要将这个数据传到DSP里,但是中间的数据传输是不是可以分好几次传的呢?
您好,我确实是要用音频ADC,请问您有这方面的例子吗,如果有的话,麻烦您发到我邮箱,谢谢!812515899@qq.com
ADC虽然是24位,但是传输的时候用16/24/32位都可以。作为Slave设备的时候,dsp设置是多少它就是多少。dsp使用McBSP接口,可以参考文档SPRU566J来编程,应该很容易找到例子。