This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5754M 使用3 wire I2S配置问题

各位大神:

  使用TAS5754需要配置成3线模式的I2S,请帮忙指导一下需要调整哪些寄存器。

 电路硬件连接如下图:

在EVM将I2S作同样硬件连接时,使用EVM Hybridflow 3配置,功放有声音输出。

 手动调整寄存器配置:

Page0:

Reg 0x25 0x5A  //Disable clock auto set;

Reg 0x0d 0x10  //PLL Reference clock is BCLK;

Reg 0x14 0x00 0x10 0x00 0x00 0x01   //设定PLL DIVIDER P, J ,D ,R

Reg 0x1b 0x01 0x0f 0x03 0x07       //DSP ,DAC,NCP, OSR CLOCK DIVIDER

这时没有声音输出。

 请指导一下上面的配置是否正确,还有哪里需要设定一下?

 另外,如果BCLK 值为1.411MHZ时,又该如何配置?

 试过将以上寄存器配置参数输入2/4/8x FIR Interp. With de-emph模式,这时有声音输出。