This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320AIC3106采集正弦波到OMAPL138问题

我用AIC3106通过左通道LINE1LP单端输入采集正弦波(LINE1LM接地),采到的波形经过3106的AD输出给OMAPL138,用32位整型数据存储(实际AD数据只有16位,因为I2S设置的是1个Slot 16bit),存到数组里面(sample_L=InputSample();   ReciveBuffer_R[count]=sample_R;) 48KHz采样频率采16K的正弦波,但是踩进来之后我不做输出使用,而是想要做一些数据处理然后把解算之后的数据送到ARM中。现在的情况是:我用CCS6.1的绘图功能把采到的量化电压数据画出来,画的图像不正确,不知道是为什么,请各位前辈帮忙解决一下

后三张图片只是显示方式不一样,一个是连线 ,一个是连线带采样点,第三个是只有采样点