This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问PCM3070的pin18(REF)的电压是如何产生的,3070内部的电源架构是怎样的?pin18和pin30(LDO-SELECT)有什么关系??
对于常用芯片的模拟部分的参考电压的生成,通常输出驱动部分来讲是使用负反馈放大器/比较器做输出推动(电压放大1:1),比较器的参考电压决定了Vref电压,这个参考电压:
1. Vmid: Vcc/2 或 Vdd/2,这种就是使用电阻分压,得到模拟电压的1/2,所以也叫Vmid.
2. Band gap电压产生Vref, 如果芯片的Vref是固定的,比如0.75, 0.9, 1.65 之类,那么通常参考电压由band gap电压分压产生。PCM3070就是使用band gap电压产生Vref,具有非常高的PSRR。缺点是成本高。
LDO-SELECT
pin18和pin30没有任何关系。
LDO-SELECT用于选择Analog和digital部分的核心电压的source是使用内部LDO还是使用外部提供。具体看ref manual