This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3101输出信号失真度大的问题

我们产品上使用DAC3101,输出信号失真度很大,达到1.86%。

 

国外一款录音器ZOOM H6,失真度只有0.0012%。

我用一个44.1k采样率的1kHz正弦波wav文件,在ZOOM H6上播放,用音频分析仪AP ATS-2测试失真度为0.0012%。(这说明wav文件正常。)

用同一个wav文件,在我们的产品上播放,AP ATS-2测试失真度很大,为1.86%。

 

请问是什么原因呢?

 

Processing Block使用PRB_7,IIR使用默认参数,

也尝试过使用PRB_1,使用默认参数,

结果失真度一样。

 

已经测试过,DAC3101的模拟调音(下图右边部分)没有问题。

测试方法是:从AIN1和AIN2输入信号,信号路由也设置这两个输入为信号源,其他信号源设置断开,测试输出端信号。失真度0.014%。

 

也检查过I2S控制信号,下图左边部分,信号时序正确,使用的是标准I2S模式。

请问,如何配置DAC3101中Processing Block的参数,才能改善信号失真度?