This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116测试问题



现在我们20W*2音响所用的TPA3116主要遇到如下两个问题,麻烦帮忙分析,急!!!

功放设计的输入电压17V;输出的2个喇叭是4ohm

1,TPA3116带载(双4 ohm)开机电流很大--->>分析:单独给TPA3116供电17VDC,开机瞬间电流超过6A;空载开机电流为60mA;

2,TPA3116保护---单独给TPA3116供电17VDC,加散热片,当双通道功率到达14.5W时功放能维持2秒就shutdown,若播放同时用风扇吹功放,14.5W时能持续,增加输出到16W时就shutdown。

另外,若SDZ和FAULTZ管脚单独上拉100K到3.3VDC时,当功放shutdown后必须要断电功放才能恢复;

若SDZ和FAULTZ先短接在上拉100K到3.3VDC时,功放shutdown后能自动恢复。

(功放输入端最大为500mVac),功放电路如下:

感谢!