请教各位专家!
如题,前端输出是L/R两路信号,需要输入给TLV320AIC3101,这颗芯片的输入是差分信号,MIC1LP/LINE1LP和MIC1LM/LINE1LM,请问有专业的芯片可以完成这个功能吗?或者直接把L/R信号混合在一起接MIC1LP/LINE1LP可以吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教各位专家!
如题,前端输出是L/R两路信号,需要输入给TLV320AIC3101,这颗芯片的输入是差分信号,MIC1LP/LINE1LP和MIC1LM/LINE1LM,请问有专业的芯片可以完成这个功能吗?或者直接把L/R信号混合在一起接MIC1LP/LINE1LP可以吗?
谢谢!
两种方案:
1.通过全差分运放比如OPA1632将单端信号转差分给AIC3101。
2.AIC3101可以是差分输入也可以是单端输入,所以不转差分的话也是可以的。
非常感谢您的回复!
AIC3101是在另外一块板卡上,目前预留的接口只有MIC1LP/LINE1LP和MIC1LM/LINE1LM,只能转成差分。
OPA1632是差分音频放大器,如果不需要放大,可以按照以下方式直接相连吗?
请问以下两种方式是否可行?
1. 把L左声道单端信号接到MIC1LP/LINE1LP,MIC1LM/LINE1LM接地
2. L左声道单端信号和R右声道单端信号混合在一起,然后接到MIC1LP/LINE1LP,MIC1LM/LINE1LM接地
如果方法2可行的话,L和R信号直接接在一起可以吗?还是有专门的芯片?谢谢!