This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3203没有输出(HPL/HPR),请给予技术支持,谢谢!



根据数据手册4.2的配置,寄存器都配置正确,但HPL和HPR没有输出

Stereo DAC Playback with 48ksps Sample Rate and Low Power Mode

Assumption: MCLK = 12.288MHz, Slave I2S
#----------- Initialize to page 0
w 30 00 00
#----------- Initialize the device through software reset
w 30 01 01
#----------- Power up the NDAC divide with value 1
w 30 0b 81
#----------- Power up the MDAC divider with value 4
w 30 0c 84
#----------- Program the OSR of DAC to 64
w 30 0d 00
w 30 0e 40
#----------- Set the DAC mode to PRB_P8
w 30 3c 08
#----------- Select page 1
w 30 00 01
#----------- Disable internal crude AVdd in presence of external AVdd supply
#----------- or before powering up internal AVdd LDO
w 30 01 08
#----------- Enable master analog power control
w 30 02 00
#----------- Set the REF charging time to 40ms
w 30 7b 01
#----------- Set the input common mode to 0.9V and output common mode for headphone
#----------- to input common mode
w 30 0a 00
#----------- Route left DAC to HPL
w 30 0c 08
#----------- Route right DAC to HPR
w 30 0d 08
#----------- Set the DAC PTM mode to PTM_P1
w 30 03 08
w 30 04 08
#----------- Set the HPL gain to 0dB
w 30 10 00
#----------- Set the HPR gain to 0dB
w 30 11 00
#----------- HP soft stepping settings for optimal pop performance at power up
#----------- Rpop used is 6k with N = 6 & soft step = 20usec.
w 30 14 29
#----------- Power up HPL and HPR drivers
w 30 09 30
#----------- Wait for 2.5 sec for soft stepping to take effect
#----------- Else read Page 1, Register 63d, D(7:6). When = “11” soft-stepping is complete
#----------- Select page 0
w 30 00 00
#----------- Power up the left and right DAC channels and route the left channel I2S data
#----------- to left channel DAC and right channel I2S data to right channel DAC
w 30 3f d4
#----------- Unmute the DAC digital volume control
w 30 40 00