This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

有没有那个AD、DA具有48K带宽,或AIC系列的具有48K带宽

如题,我现在想在153.6K的采样频率下实现48K的带宽,有没有可以推荐的AD、DA。

还有AIC系列的有实现48K的带宽的吗?

谢谢了

  • ADC 与 DAC 的参数是: 通道数,精度,供电电压等。可到这里找找:http://www.ti.com/data-converters/adc-circuit/high-speed/overview.html

    另外:  AIC 系列 48K 双通道, 所有系列基本都能满足

  • 你好,我手上的C5517EVM上具有AIC3204,但是该芯片在153.6k的采样率下,仅仅只能实现20K多的带宽。难道是我设置的问题?

    类似AIC3204的芯片,但是在153.6K采样率的条件下,能实现48K的带宽。能给推荐下吗?

    多谢了!

  • 那你手头上有没有其他AD,DA芯片,不是audio应用的,因为AIC3204等是audio应用上的,我想是因为限制在音频信号带宽范围,20~20KHz,所以测试得到只有20KHz左右带宽。 但是按照奈奎斯特定理,达到48KHz带宽是没问题的。 

    所以如果您手头上有其他应用AD,或者DA 芯片,可以试下。