This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我购买了AIC3262开发板,折腾好多天才知道大概要怎么调试,但是还是不大熟练。我调试时操作一般如下:
1,把开发板连接到电脑;
2,运行CodecControl,设置一下audio path和power开关;
3,运行GDE,打开之前编辑好的pfw文件,在build菜单里选“download and run”
我发现几个疑问:
1,我编辑好的CodecControl的audio path和power开关设置,怎样可以保留下来,不用每次都重新设置一遍?
2,每次“download and run” 编辑好的pfw,都需要重新汇编一次挺占时间,难道以前的汇编结果都不在了吗?
3,CodecControl和GDE可以同时在电脑上一直打开吗?两者同时访问开发板会不会存在打架现象?我发现跑完上面3步,经常有些设置开关虽然在界面上显示是打开的,但实际好像不起作用,需要在两个工具中来回刷几下,才起作用,所以怀疑是不是因为我同时打开两个工具导致对开发板的设置有冲突。
4,假设我在CodecControl中已经调试好path,power开关;在GDE中调试好DSP并且产生了DSP的cfg文件,那最后我应该怎样把两个工具的调试结果合二为一,生成一个最终用于产品化的配置文件?