This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3251容易损坏,紧急求助!!!

你好!我使用官方电路PBTL模式设计的PCB,当我用焊台焊接好芯片后,上电发现无任何输出,其中一路输出是DC10.5V左右(我GVDD供电是11.5V,PVDD供电是35.6V,这时VDD是3.256V,AVDD是7.66V,VGB是1.2V,rest是2.8V),另一路输出是0.545V,功放不起震,两个故障指示脚为均低电平。

当我用热风枪拆掉这个故障芯片再使用热风枪更换一个新的IC,这个IC有方波输出了(这时VDD是3.256V,AVDD是7.66V,VGB是1.2V,rest是2.8V),当我使用焊台的烙铁补焊一下PVDD那边一整排引脚后,再次上电功放不起震,两组输出均是DC10.5V,功放不起震,两个故障指示脚为均低电平。这样反复操作已经损坏6片芯片了,在这期间试过把烙铁接地,试过把烙铁拔电后再焊接,均以失败告终,现象均是输出DC10.5V,功放不起震,有时只有一路是输出直流10.5V,有时是两路。

请教下大家,这究竟是怎么一回事啊?这个IC很脆弱吗?我用过的TPA3116就没有这种问题。希望能有人尽快解答下我,在线等。先谢谢大家了!

x 出现错误。请重试或与管理员联系。