一片CPU用3片TLV320AIC3254做音频处理,想用一路I2C总线对其配置可行吗?
TLV320AIC3254 Application Reference Guide中
The TLV320AIC3254 supports the I2C control protocol, and will respond to the I2C address of 0011000.
I2C is a two-wire, open-drain interface supporting multiple devices and masters on a single bus
Each device on an I2C bus has a unique 7-bit
address to which it responds. (Slaves can also have 10-bit addresses; see the I2C specification for
details.)
地址好像是唯一的 0011000没法设置,手册中又提到可使用10位地址但是没找到说明怎样用,哪位大侠用过