This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用的48V作功率电源。BTL,负载4欧姆。配上散热器,加风扇。功率推到2x130就不能再推了。1K的信号,还没削顶失真。。。。SD关断了功放输出。这个片子大概可以到2x300W的嘛。差太多了。单独只接一路BTL的时候,另一路不接。能到280W左右,都不会关断,这时候信号削顶了的。负载电阻也没有出现短路现象。温度也还没报警。48V电压也没掉。为啥SD会工作?求工作人员解答
您的意思SD引脚输出为低时,输出还是有功率输出的是吗?
功率只能到130W时候,看下OTW1,OTW2的输出情况?
另外,建议把电路附上,以便分析。