Other Parts Discussed in Thread: TPA3251
您好!
最近在用TPA3251做D类功放,其负载是电感线圈,工作频率在20K.
输入信号为Vpp=2v的正弦波信号,采用PBTL形式。由于输出电压不够,采用了变压器升压后再加到电感线圈上。电感负载在1mH左右,但是在实际测试过程中发现以下几点问题:
1.带上不同负载,1mH和1.5mH的负载,其电压幅值差别很大;
2.滤波电感是不是就在10uH左右比较好,因为刚开始设计到18uH和0.47UF,输出的电压发生畸变。后来修成后,波形得到改善;
3.datasheet中提到的输出功率,是视在功率还是有功功率?通过计算有功功率只有不到20W,但是发热也不小。
谢谢!