This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3118 引脚定义问题

请教TI的工程师们:

TPA3118 功放芯片几个管脚是如何定义的:

1、Pin1为MODSEL功能,高低电平分别为:1SPW模式与BD模式,请教这两种模式的差异是什么?应该怎么去选择?规格书上没有说明;

2、Pin8为GAIN/SLV功能,涉及到主从模式的增益配置,主模式和从模式是如何设置的?是直接以配置电阻的方式来做判断?还是另外有

      有其他的配置引脚?

3、BOOST引脚在功放工作的时候,电压提升会非常高,瞬间可达到100多V,这个Boost电容的耐压选择有何要求?参考设计的只有25V

      耐压,是否有问题?

4、功放输出到喇叭之间,有两个RC滤波电路,常规的推荐电容都是0.1uF,TPA3118设计选择0.01uF,是处于何种原因考虑的?

5、Pin12 Mute功能,此为高电平静音状态,上电容易控制,在播放音乐的时候断电就很难进行先Mute操作,会产生POP冲击声,有没有什么办法解决?

非常感谢!