This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3118计算输出功率?

你好!万能的TI工程师

我在使用TPA3118时,想了解下如何计算,输出电压,比如24V电压时,PLIMIT和GVDD是连在一起的(是7V对吗?),喇叭使用4Ω的,请问图中的Rs和Vp是如果得知的?POUT是1%的功率吗?Pout*1.25是10%的输出功率吗?

请告知

谢谢!