This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

5509的AIC23问题

想用5509实现mic输入phone口输出声音,但是这个程序没有反应,调试的时候也没有显示错误,不知道是什么原因?请问该如何解决,另外我用的是ccs3.3基于XP虚拟机做的

/*
 * Copyright (C) 2003 Texas Instruments Incorporated
 * All Rights Reserved
 */
/*
 *---------main_dma4.c---------
 * This example places the MCBSP in digital loopback mode and
 * syncs MCBSP receive with DMA channel 4 and MCBSP transmit
 * with DMA channel 5.                                       
 * The example uses predefined CSL macros and symbolic       
 * constants to create the initialization values needed for  
 * the MCBSP and DMA control registers to effect the transfer
 */
#include <stdio.h>
#include <csl.h>
#include <csl_i2c.h>
#include <math.h>
#include <csl_pll.h>
#include <csl_mcbsp.h>
#include <csl_dma.h>
#include <csl_irq.h>


//---------Global constants---------
#define N       512
#define CODEC_ADDR 0x1A     //AIC23在I2C总线上的从地址0011010
int TestflagR=0;
int TestflagT=0;
Uint16 i2c_status;



//---------Global data definition---------

/* Define transmit and receive buffers */
#pragma DATA_SECTION(xmt,"dmaMem")
Uint16 xmt[N];
#pragma DATA_SECTION(rcv,"dmaMem")
Uint16 rcv[N];

/*锁相环的设置*/
PLL_Config  myConfig      = {
  0,    //IAI: the PLL locks using the same process that was underway
                //before the idle mode was entered
  1,    //IOB: If the PLL indicates a break in the phase lock,
                //it switches to its bypass mode and restarts the PLL phase-locking
                //sequence
  24,    //PLL multiply value; multiply 24 times
  1             //Divide by 2 PLL divide value; it can be either PLL divide value
                //(when PLL is enabled), or Bypass-mode divide value
                //(PLL in bypass mode, if PLL multiply value is set to 1)
};

/*******************************************************************************************/
/**********************************MCBSP设置************************************************/


  MCBSP_Config ConfigLoopBack16= {
MCBSP_SPCR1_RMK(
    MCBSP_SPCR1_DLB_OFF,                   /* DLB    = 0,禁止自闭环方式 */
    MCBSP_SPCR1_RJUST_LZF,                 /* RJUST  = 2 */
    MCBSP_SPCR1_CLKSTP_DISABLE,            /* CLKSTP = 0 */
    MCBSP_SPCR1_DXENA_ON,                  /* DXENA  = 1 */
    0,                                     /* ABIS   = 0 */
    MCBSP_SPCR1_RINTM_RRDY,                /* RINTM  = 0 */
    0,                                     /* RSYNCER = 0 */
    MCBSP_SPCR1_RRST_DISABLE               /* RRST   = 0 */
   ),
    MCBSP_SPCR2_RMK(
    MCBSP_SPCR2_FREE_NO,                   /* FREE   = 0 */
    MCBSP_SPCR2_SOFT_NO,                   /* SOFT   = 0 */
    MCBSP_SPCR2_FRST_FSG,                  /* FRST   = 0 */
    MCBSP_SPCR2_GRST_CLKG,                 /* GRST   = 0 */
    MCBSP_SPCR2_XINTM_XRDY,                /* XINTM  = 0 */
    0,                                     /* XSYNCER = N/A */           
    MCBSP_SPCR2_XRST_DISABLE               /* XRST   = 0 */
   ),
   /*单数据相,接受数据长度为16位,每相2个数据*/
  MCBSP_RCR1_RMK(
      MCBSP_RCR1_RFRLEN1_OF(1),              /* RFRLEN1 = 1 */
      MCBSP_RCR1_RWDLEN1_16BIT               /* RWDLEN1 = 2 */
  ),
  MCBSP_RCR2_RMK(    
    MCBSP_RCR2_RPHASE_SINGLE,              /* RPHASE  = 0 */
    MCBSP_RCR2_RFRLEN2_OF(0),              /* RFRLEN2 = 0 */
    MCBSP_RCR2_RWDLEN2_8BIT,               /* RWDLEN2 = 0 */
    MCBSP_RCR2_RCOMPAND_MSB,               /* RCOMPAND = 0 */
    MCBSP_RCR2_RFIG_YES,                   /* RFIG    = 0 */
    MCBSP_RCR2_RDATDLY_1BIT                /* RDATDLY = 1 */
    ),  
   MCBSP_XCR1_RMK(    
    MCBSP_XCR1_XFRLEN1_OF(1),              /* XFRLEN1 = 1 */
    MCBSP_XCR1_XWDLEN1_16BIT               /* XWDLEN1 = 2 */
    
 ),   
 MCBSP_XCR2_RMK(   
    MCBSP_XCR2_XPHASE_SINGLE,              /* XPHASE  = 0 */
    MCBSP_XCR2_XFRLEN2_OF(0),              /* XFRLEN2 = 0 */
    MCBSP_XCR2_XWDLEN2_8BIT,               /* XWDLEN2 = 0 */
    MCBSP_XCR2_XCOMPAND_MSB,               /* XCOMPAND = 0 */
    MCBSP_XCR2_XFIG_YES,                   /* XFIG    = 0 */
    MCBSP_XCR2_XDATDLY_1BIT                /* XDATDLY = 1 */
  ),            
 MCBSP_SRGR1_DEFAULT,
 MCBSP_SRGR2_DEFAULT,  
 MCBSP_MCR1_DEFAULT,
 MCBSP_MCR2_DEFAULT,
 MCBSP_PCR_RMK(
   MCBSP_PCR_IDLEEN_RESET,                 /* IDLEEN   = 0   */
   MCBSP_PCR_XIOEN_SP,                     /* XIOEN    = 0   */
   MCBSP_PCR_RIOEN_SP,                     /* RIOEN    = 0   */
   MCBSP_PCR_FSXM_EXTERNAL,                /* FSXM     = 0   */
   MCBSP_PCR_FSRM_EXTERNAL,                /* FSRM     = 0   */
   0,                                      /* DXSTAT = N/A   */
   MCBSP_PCR_CLKXM_INPUT,                  /* CLKXM    = 0   */
   MCBSP_PCR_CLKRM_INPUT,                  /* CLKRM    = 0   */
   MCBSP_PCR_SCLKME_NO,                    /* SCLKME   = 0   */
   MCBSP_PCR_FSXP_ACTIVEHIGH,              /* FSXP     = 0   */
   MCBSP_PCR_FSRP_ACTIVEHIGH,              /* FSRP     = 1   */
   MCBSP_PCR_CLKXP_FALLING,                /* CLKXP    = 1   */
   MCBSP_PCR_CLKRP_RISING                  /* CLKRP    = 1   */
 ),
 MCBSP_RCERA_DEFAULT,
 MCBSP_RCERB_DEFAULT,
 MCBSP_RCERC_DEFAULT,
 MCBSP_RCERD_DEFAULT,
 MCBSP_RCERE_DEFAULT,
 MCBSP_RCERF_DEFAULT,
 MCBSP_RCERG_DEFAULT,
 MCBSP_RCERH_DEFAULT,
 MCBSP_XCERA_DEFAULT,
 MCBSP_XCERB_DEFAULT,
 MCBSP_XCERC_DEFAULT,
 MCBSP_XCERD_DEFAULT,  
 MCBSP_XCERE_DEFAULT,
 MCBSP_XCERF_DEFAULT,  
 MCBSP_XCERG_DEFAULT,
 MCBSP_XCERH_DEFAULT
};     

 
 /*******************************************************************************************/
/************************************DMA设置************************************************/


/* Create DMA Receive Side Configuration */
DMA_Config  dmaRcvConfig = {
  DMA_DMACSDP_RMK(

    DMA_DMACSDP_DSTBEN_NOBURST,    //Destination burst :-不使用突发
    DMA_DMACSDP_DSTPACK_OFF,       //Destination packing :-目标口禁止打包
    DMA_DMACSDP_DST_DARAM,         //Destination selection :-接收的目标口是DARAM
    DMA_DMACSDP_SRCBEN_NOBURST,    //Source burst :-源突发禁止
    DMA_DMACSDP_SRCPACK_OFF,       //Source packing :-源口禁止打包
    DMA_DMACSDP_SRC_PERIPH,        //Source selection :-外设mcbsp
    DMA_DMACSDP_DATATYPE_16BIT     //Data type :-设置数据类型16bit字长

  ),                                /* DMACSDP 源与目标参数寄存器 */

  DMA_DMACCR_RMK(

    DMA_DMACCR_DSTAMODE_POSTINC,    //Destination address mode :-自动执行后增量(由于本程序中数据类型是16bit,所以+2)
    DMA_DMACCR_SRCAMODE_CONST,      //Source address mode :-源地址为恒定地址
    DMA_DMACCR_ENDPROG_ON,          //End of programmation bit :-

    DMA_DMACCR_REPEAT_ON,           //Repeat condition :-不管编程配置结束位,结束传输自动初始化开始

    //DMA_DMACCR_REPEAT_OFF,
    DMA_DMACCR_AUTOINIT_ON,         //Auto initialization bit :-
    //DMA_DMACCR_AUTOINIT_OFF,
    DMA_DMACCR_EN_STOP,             //Channel enable :-设置时先关闭通道
    DMA_DMACCR_PRIO_LOW,            //Channel priority :-设置为低优先级
    DMA_DMACCR_FS_ELEMENT,          //Frame/Element Sync :-单元事件同步
    //DMA_DMACCR_FS_DISABLE,
    DMA_DMACCR_SYNC_REVT0           //Synchronization control :-McBSP1 Receive Event(REVT1)

  ),                                       /* DMACCR 通道控制寄存器  */

  DMA_DMACICR_RMK(

    DMA_DMACICR_BLOCKIE_ON,       //Whole block interrupt enable :-块传输完成后中断使能
    //DMA_DMACICR_BLOCKIE_OFF,
    DMA_DMACICR_LASTIE_OFF,       //Last frame interrupt enable :-
    DMA_DMACICR_FRAMEIE_OFF,      //Whole frame interrupt enable :-
    //DMA_DMACICR_FRAMEIE_ON,
    DMA_DMACICR_FIRSTHALFIE_OFF,  //Half frame interrupt enable :-
    DMA_DMACICR_DROPIE_OFF,       //Sync. event drop interrupt enable :-
    DMA_DMACICR_TIMEOUTIE_OFF     //Time out interrupt enable :-

  ),                                       /* DMACICR 中断控制寄存器 */

    (DMA_AdrPtr)(MCBSP_ADDR(DRR10)),       /* DMACSSAL 源地址低位 */
    0,                                     /* DMACSSAU 源地址高位*/
    (DMA_AdrPtr)&rcv,                  /* DMACDSAL 目的地址低位*/
    0,                                     /* DMACDSAU 目的地址高位*/
    2,                                     /* DMACEN   1 帧内数据长度 16*2 两个数据一个帧*/
    N/2,                                   /* DMACFN  帧数大小 */
    0,                                     /* DMACFI  */
    0                                      /* DMACEI  */

  };

/* Create DMA Transmit Side Configuration */
DMA_Config  dmaXmtConfig = {
  DMA_DMACSDP_RMK(

    DMA_DMACSDP_DSTBEN_NOBURST,    //Destination burst :-不使用突发
    DMA_DMACSDP_DSTPACK_OFF,       //Destination packing :-目标口禁止打包
    DMA_DMACSDP_DST_PERIPH,        //Destination selection :-接收的目标口是外设mcbsp
    DMA_DMACSDP_SRCBEN_NOBURST,    //Source burst :-源突发禁止
    DMA_DMACSDP_SRCPACK_OFF,       //Source packing :-源口禁止打包
    DMA_DMACSDP_SRC_DARAM,         //Source selection :源口为DARAM
    DMA_DMACSDP_DATATYPE_16BIT     //Data type :-设置数据类型16bit字长

  ),                                       /* DMACSDP  源与目标参数寄存器 */

  DMA_DMACCR_RMK(

    DMA_DMACCR_DSTAMODE_CONST,    //Destination address mode :-目标口地址为恒定地址
    DMA_DMACCR_SRCAMODE_POSTINC,  //Source address mode :-自动执行后增量(由于本程序中数据类型是16bit,所以+2)
    DMA_DMACCR_ENDPROG_ON,        //End of programmation bit :-

    DMA_DMACCR_REPEAT_ON,         //Repeat condition :-不管编程配置结束位,结束传输自动初始化开始

    //DMA_DMACCR_REPEAT_OFF,
    DMA_DMACCR_AUTOINIT_ON,       //Auto initialization bit :-
    //DMA_DMACCR_AUTOINIT_OFF,
    DMA_DMACCR_EN_STOP,           //Channel enable :-设置时先关闭通道
    DMA_DMACCR_PRIO_LOW,          //Channel priority :-设置为低优先级
    DMA_DMACCR_FS_ELEMENT,        //Frame/Element Sync :-单元事件同步
    //DMA_DMACCR_FS_DISABLE,
    DMA_DMACCR_SYNC_XEVT0         //Synchronization control :-McBSP1 Transmit Event(XEVT1)
  ),                                       /* DMACCR 通道控制寄存器   */

  DMA_DMACICR_RMK(

    DMA_DMACICR_BLOCKIE_ON,       //Whole block interrupt enable :-块传输完成后中断使能
    //DMA_DMACICR_BLOCKIE_OFF,
    DMA_DMACICR_LASTIE_OFF,       //Last frame interrupt enable :-
    DMA_DMACICR_FRAMEIE_OFF,       //Whole frame interrupt enable :-
    //DMA_DMACICR_FRAMEIE_ON,
    DMA_DMACICR_FIRSTHALFIE_OFF,  //Half frame interrupt enable :-
    DMA_DMACICR_DROPIE_OFF,       //Sync. event drop interrupt enable :-
    DMA_DMACICR_TIMEOUTIE_OFF     //Time out interrupt enable :-

  ),                                       /* DMACICR 中断控制寄存器 */

    (DMA_AdrPtr)&xmt[0],               /* DMACSSAL 源地址低位*/
    0,                                     /* DMACSSAU 源地址高位 */
    (DMA_AdrPtr)(MCBSP_ADDR(DXR10)),       /* DMACDSAL 目的地址低位*/
    0,                                     /* DMACDSAU 目的地址高位*/
    2,                                     /* DMACEN   1 帧内数据长度 16*2 两个数据一个帧*/
    N/2,                                   /* DMACFN  帧数大小  */
    0,                                     /* DMACFI   */
    0                                      /* DMACEI   */

};


/* Define a DMA_Handle object to be used with DMA_open function */
DMA_Handle hDmaRcv, hDmaXmt;

/* Define a MCBSP_Handle object to be used with MCBSP_open function */
MCBSP_Handle hMcbsp;

volatile Uint16 transferComplete = FALSE;
Uint16 err = 0;
Uint16 old_intm;
Uint16 xmtEventId, rcvEventId;

//---------Function prototypes---------
/* Reference start of interrupt vector table   */
/* This symbol is defined in file, vectors.s55 */
extern void VECSTART(void);

/* Protoype for interrupt functions */
interrupt void dmaXmtIsr(void);
interrupt void dmaRcvIsr(void);
void taskFxn(void);



/*******************************************************************************************/
/***********************************I2C的设置和AIC的设置************************************/



/* This next struct shows how to use the I2C API */
/* Create and initialize an I2C initialization structure */
I2C_Setup I2Cinit = {
        0,              /* 7 bit address mode */
        0,         /* own address - don't care if master */
        144,            /* clkout value (Mhz)  */
        50,            /* a number between 10 and 400*/
        0,              /* number of bits/byte to be received or transmitted (8)*/
        0,              /* DLB mode on*/
        1               /* FREE mode of operation on*/
};


/*数字音频接口格式设置
AIC23为主模式,数据为DSP模式,数据长度16位*/   
Uint16 digital_audio_inteface_format[2]={0x0e,0x53};
/*AIC23的波特率设置,采样率为44.1K*/
Uint16 sample_rate_control[2] = {0x10,0x23};
/*AIC23寄存器复位*/
Uint16 reset[2] ={0x1e,0x00};
/*AIC23节电方式设置,所有部分均所与工作状态*/
Uint16 power_down_control[2] ={0x0c,0x00};

/*AIC23模拟音频的控制
DAC使能,ADC输入选择为mic*/
Uint16 analog_aduio_path_control[2] ={0x08,0x10};
//Uint16 analog_aduio_path_control[2] ={0x08,0x15};//MIC IN 有增益
//Uint16 analog_aduio_path_control[2] ={0x08,0x14};//MIC IN 无增益
//Uint16 analog_aduio_path_control[2] ={0x08,0x10};//Line IN

/*AIC23数字音频通路的控制*/
Uint16 digital_audio_path_control[2] ={0x0a,0x05};
/*AIC23数字接口的使能*/
Uint16 digital_interface_activation[2] ={0x12,0x01};
/*AIC23左通路音频调节*/
Uint16 left_line_input_volume_control[2] ={0x00,0x17};
/*AIC23右通路音频调节*/
Uint16 right_line_input_volume_control[2] ={0x02,0x17};
/*AIC23耳机左通路音频调节*/
Uint16 left_headphone_volume_control[2] ={0x05,0xFF};
/*AIC23耳机右通路音频调节*/
Uint16 right_headphone_volume_control[2] = {0x07,0xFF};



/*******************************************************************************************/
/*******************************************************************************************/



void delay(Uint32 k)
{
   while(k--);
}



/*******************************************************************************************/
/*******************************************************************************************/



void CODEC(void)
{
    //printf ("%s\n","CODEC");
    /*I2C is undet reset*/
    I2C_RSET(I2CMDR,0);
    /*设置预分频寄存器,I2C的mode clock is 10MHz*/
    delay(100);
    I2C_RSET(I2CSAR,0x001A);
    I2C_RSET(I2CMDR,0x0620);    
    I2C_setup(&I2Cinit);
      /*设置I2C的Mater clock*/
    I2C_RSET(I2CCLKL,100);
    I2C_RSET(I2CCLKH,100);



    /*reset AIC23*/
    i2c_status = I2C_write( reset,          //pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
    delay(1000);
    /*设置AIC23各部分均工作*/
    i2c_status = I2C_write( power_down_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );            
    /*设置AIC23的数字接口*/
    i2c_status = I2C_write( digital_audio_inteface_format,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                               );
     /*设置AIC23模拟通路*/
    i2c_status = I2C_write( analog_aduio_path_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
    /*设置数字通路*/
    i2c_status = I2C_write( digital_audio_path_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                              );        
    /*设置AIC23的采样率*/
    i2c_status = I2C_write( sample_rate_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
    /*设置耳机音量*/
    i2c_status = I2C_write( left_headphone_volume_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
    i2c_status = I2C_write( right_headphone_volume_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );  
    /*设置Line输入的音量*/
    i2c_status = I2C_write( left_line_input_volume_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
    i2c_status = I2C_write( right_line_input_volume_control,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
    /*启动AIC23*/
    i2c_status = I2C_write( digital_interface_activation,//pointer to data array
                            2,                //length of data to be transmitted
                            1,                //master or slaver
                            CODEC_ADDR,        //slave address to transmit to
                            1,                //transfer mode of operation
                            30000            //time out for bus busy
                            );
}




//---------main routine---------
void main(void)
{
    Uint16 i;

    /* Initialize CSL library - This is REQUIRED !!! */
    CSL_init();
    /* Set IVPD/IVPH to start of interrupt vector table */
    IRQ_setVecs((Uint32)(&VECSTART));
    PLL_config(&myConfig);

    /* Call function to effect transfer */
    CODEC();
    taskFxn();
    
}

void taskFxn(void)
{
    Uint16 srcAddrHi, srcAddrLo;
    Uint16 dstAddrHi, dstAddrLo;
    Uint16 i;
 
    /* By default, the TMS320C55xx compiler assigns all data symbols word */
    /* addresses. The DMA however, expects all addresses to be byte       */
    /* addresses. Therefore, we must shift the address by 2 in order to   */
    /* change the word address to a byte address for the DMA transfer.    */
    srcAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DRR10))) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DRR10))) << 1) & 0xFFFFu;
    dstAddrHi = (Uint16)(((Uint32)(&rcv)) >> 15) & 0xFFFFu;
    dstAddrLo = (Uint16)(((Uint32)(&rcv)) << 1) & 0xFFFFu;

    dmaRcvConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
    dmaRcvConfig.dmacssau = srcAddrHi;
    dmaRcvConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaRcvConfig.dmacdsau = dstAddrHi;

    srcAddrHi = (Uint16)(((Uint32)(&xmt[0])) >> 15) & 0xFFFFu;
    srcAddrLo = (Uint16)(((Uint32)(&xmt[0])) << 1) & 0xFFFFu;
    dstAddrHi = (Uint16)(((Uint32)(MCBSP_ADDR(DXR10))) >> 15) & 0xFFFFu;
    dstAddrLo = (Uint16)(((Uint32)(MCBSP_ADDR(DXR10))) << 1) & 0xFFFFu;

    dmaXmtConfig.dmacssal = (DMA_AdrPtr)srcAddrLo;
    dmaXmtConfig.dmacssau = srcAddrHi;
    dmaXmtConfig.dmacdsal = (DMA_AdrPtr)dstAddrLo;
    dmaXmtConfig.dmacdsau = dstAddrHi;

    /* Open MCBSP Port 1 and set registers to their power on defaults */
    hMcbsp = MCBSP_open(MCBSP_PORT0, MCBSP_OPEN_RESET);

    /* Open DMA channels 4 & 5 and set regs to power on defaults */
    hDmaRcv = DMA_open(DMA_CHA4,DMA_OPEN_RESET);
    hDmaXmt = DMA_open(DMA_CHA5,DMA_OPEN_RESET);  

    /* Get interrupt event associated with DMA receive and transmit */
    xmtEventId = DMA_getEventId(hDmaXmt);
    rcvEventId = DMA_getEventId(hDmaRcv);
    
    /* Temporarily disable interrupts and clear any pending */
    /* interrupts for MCBSP transmit */
    old_intm = IRQ_globalDisable();
    
    /* Clear any pending interrupts for DMA channels */
    IRQ_clear(xmtEventId);
    IRQ_clear(rcvEventId);

    /* Enable DMA interrupt in IER register */
    IRQ_enable(xmtEventId);
    IRQ_enable(rcvEventId);

    /* Set Start Of Interrupt Vector Table */
    IRQ_setVecs(0x10000);
    
    /* Place DMA interrupt service addresses at associate vector */
    IRQ_plug(xmtEventId,&dmaXmtIsr);
    IRQ_plug(rcvEventId,&dmaRcvIsr);

    /* Write values from configuration structure to MCBSP control regs */
    MCBSP_config(hMcbsp, &ConfigLoopBack16);
    
    /* Write values from configuration structure to DMA control regs */
    DMA_config(hDmaRcv,&dmaRcvConfig);
    DMA_config(hDmaXmt,&dmaXmtConfig);

#if 0  
    /* Take MCBSP transmit and receive out of reset */
    MCBSP_start(hMcbsp,
                MCBSP_XMIT_START | MCBSP_RCV_START,
                0u);
 
    /* Prime MCBSP DXR */
    while (!(MCBSP_xrdy(hMcbsp))){
      ;
    }
    MCBSP_write16(hMcbsp,xmt[0]);
   
   /* Enable all maskable interrupts */
    IRQ_globalEnable();
   
    /* Enable DMA */
    DMA_start(hDmaRcv);
    DMA_start(hDmaXmt);
        
    /* Start Sample Rate Generator and Enable Frame Sync */
    MCBSP_start(hMcbsp,
                MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
                0x300u);
    printf ("%s\n""IF");
#else
    /* Enable all maskable interrupts */
    IRQ_globalEnable();
    
    /* Start Sample Rate Generator and Enable Frame Sync */
    MCBSP_start(hMcbsp,
                MCBSP_SRGR_START | MCBSP_SRGR_FRAMESYNC,
                0x300u);
                
    /* Enable DMA */
    DMA_start(hDmaRcv);
    DMA_start(hDmaXmt);
    
    /* Take MCBSP transmit and receive out of reset */
    MCBSP_start(hMcbsp,
                MCBSP_XMIT_START | MCBSP_RCV_START,
                0u);
    printf ("%s\n","ELSE");
#endif


   //while(DMA_FGETH(hDmaRcv, DMACCR, ENDPROG));  
    /* Wait for DMA transfer to be complete */
   //DMA_FSETH(hDmaRcv, DMACCR, ENDPROG,1);
   //DMA_FSETH(hDmaXmt, DMACCR, ENDPROG,1);
   //printf ("%s\n","AGAIN");






    //while(DMA_FGETH(hDmaRcv, DMACCR, ENDPROG));    
    //DMA_FSETH(hDmaRcv, DMACCR, ENDPROG,1);
    //DMA_FSETH(hDmaXmt, DMACCR, ENDPROG,1);
    //printf ("%s\n",err?"TEST FAILED" : "TEST PASSED");


    /* Restore status of global interrupt enable flag */
    //IRQ_globalRestore(old_intm);
        
    /* We're done with MCBSP and DMA , so close them */
    //MCBSP_close(hMcbsp);
    //DMA_close(hDmaRcv);
    //DMA_close(hDmaXmt);                     
}

interrupt void dmaXmtIsr(void) {
   Uint16 i;
   //DMA_stop(hDmaXmt);
   //IRQ_disable(xmtEventId);
   //printf ("%s\n","dmaXmtIsr");
   //DMA_start(hDmaRcv);
   //DMA_start(hDmaXmt);
   TestflagT++;

}

interrupt void dmaRcvIsr(void) {
   //DMA_stop(hDmaRcv);
   //IRQ_disable(rcvEventId);
   
   //printf ("%s\n","dmaRcvIsr");
   Uint16 i;
   //DMA_start(hDmaRcv);
   //DMA_start(hDmaXmt);
   for(i = 0; i <= N - 1; i++)
   {
        xmt[i]=rcv[i];
    }
    //DMA_start(hDmaRcv);
   DMA_start(hDmaXmt);

   TestflagR++;

   
   
}