Other Parts Discussed in Thread: TAS5711, TAS5731, TAS5704
TAS5711规格书中搭配的喇叭是8欧姆的喇叭,当搭配4欧姆的喇叭,输出电感应该时如何选择?2个输出电感上的跨接电容如何选择?是否有公式可以参考?请赐教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,对于LC的选择,可以参看下面的文档。
您好,在考虑LC设计的同时,也要考虑下电源-负载配置对效率和散热的影响。这是功放设计普遍的问题,不仅仅局限于TAS5711。桥接4ohm负载对此是比较挑战的,尤其对于像18V、24V供电时。可以对电源-负载进行适当的调整,或者使用内部Rdson更低的IC,TAS5731和TAS5711引脚兼容,Rdson降低为75m ohm。
我查看过5711的规格书,里面推荐的LC参数为15uH 0.68uF
您提供的资料中的公式为C=1/(w0*RL*1.4) L=(RL*1.4)/w0
w0的选取是如何选取的呢,有公式可以算还是经验值来的??
上述2个公式是否都使用于AD和BD 这2个工作模式??
AD和BD是传统的class D和filter-free class D两种,当前的class D大部分已经是filter-free了,即为BD了,Wo=2*pi*f,f是cut-off frequency,在此处的话,w0有点经验的性质,从文档后续可以看到其也主要基于THD来对f进行选择的,建议你可以采用文档上的表格中15uH和1.8uF。
您好:
我使用的是tas5704,我按照EVM自己画了一块板,做出板调试后,现在是输出时,只有PWM方波,接扬声器没有声音!请大神有时间的话,帮忙对照着EVM看看我画的板,有什么问题,我的毕业论文方向,先拜谢啦!如果可以的话,回复我,我把电路图给您!
你好 发你的原理图给我吧 我帮你看下 邮箱249039808@qq.com
请参考附件的计算文档, LC的选择有两个方面:
1. Fc,一般30-40k
2. Q值,不同喇叭时候的Q值不同,微调LC使得Fc附近的频响应平直。