您好,
附件是我的線路圖 & 我設定的代碼.
Mic 輸入 IN1 R, 而IN1 L 接地. Mic Bias外接
BT speaker 訊號輸入到 IN2L & IN2R
如果我單獨Mic輸入回放, 沒有雜音.
單獨BT Speaker輸入回放, 也沒有雜音.
可是我同使打開了MIC & BT speaker輸入回放, 就會有噪音, 不知道有甚麼建議. 謝謝!
還想請教一下, 我的input routing 應該怎麼設定比較好, 我發現打開CM1L, IN2L/R才有聲音, 但是就會有噪聲.
static const RegValue RecordingBothOn[] = {
//{0x00, 0x01}, //# switch to page1
//{0x33, 0x40}, //# Enable MICBIAS and set to 1.25V, MICBIAS voltage is generated from AVDD
{0x00, 0x00},
{0x3D, 0x01},
{0x00, 0x01},
{0x01, 0x08},
{0x02, 0x00},
{0x3D, 0x00},
{0x47, 0x32},
{0x7B, 0x01},
{0x00, 0x01},
{0x33, 0x00}, //40
#ifdef CONFIG_TARGET_BOARD_R1_PRO
// {0x34, 0x33}, //# IN1R, IN2L is routed to Left MICPGA POSITIVE with 40K resistance
// {0x36, 0xF0}, //# IN2R CM1L, is routed to Left MICPGA NEGATIVE with 40K resistance
// {0x37, 0xF0}, //# IN1R, IN2R is routed to Right MICPGA POSITIVE with 40K resistance
// {0x39, 0xCC}, //# , CM1L is routed to Right MICPGA NEGATIVE with 40K resistance
//{0x34, 0x22}, //# IN1R, IN2L is routed to Left MICPGA POSITIVE with 40K resistance
//{0x36, 0xA2}, //# IN2R CM1L, is routed to Left MICPGA NEGATIVE with 40K resistance
//{0x37, 0xA2}, //# IN1R, IN2R is routed to Right MICPGA POSITIVE with 40K resistance
//{0x39, 0x82}, //# , CM1L is routed to Right MICPGA NEGATIVE with 40K resistance
//{0x34, 0x02}, //# only mic /20K
//{0x36, 0x82}, //#
//{0x37, 0x80}, //#
//{0x39, 0x82}, //#
//{0x34, 0x20}, //# only BT /20K
//{0x36, 0x20}, //#
//{0x37, 0x22}, //#
//{0x39, 0x00}, //#
{0x34, 0xf3}, //0x55 //0x8a
{0x36, 0xf3},
{0x37, 0xf3}, //0x44 //0x88
{0x39, 0xf3},
#endif
#ifdef CONFIG_TARGET_BOARD_10C_EVO
#if 0 // 20K
{0x34, 0x0A}, //# IN1R, IN3L is routed to Left MICPGA POSITIVE with 40K resistance
{0x36, 0x8A}, //# IN3R, CM1L, is routed to Left MICPGA NEGATIVE with 40K resistance
{0x37, 0x88}, //# IN1R, IN3R is routed to Right MICPGA POSITIVE with 40K resistance
{0x39, 0x8A}, //# IN3L, CM1L is routed to Right MICPGA NEGATIVE with 40K resistance
#else // 40K
{0x34, 0x0F}, //# IN1R, IN3L is routed to Left MICPGA POSITIVE with 40K resistance
{0x36, 0xCF}, //# IN3R, CM1L, CM2L is routed to Left MICPGA NEGATIVE with 40K resistance
{0x37, 0xCC}, //# IN1R, IN3R is routed to Right MICPGA POSITIVE with 40K resistance
{0x39, 0xCF}, //# IN3L, CM1L, CM2L is routed to Right MICPGA NEGATIVE with 40K resistance
#endif
#endif
{0x3B, 0x28}, //# Left MICPGA Gain is enabled, Left MICPGA Gain is set to 0dB 08
{0x3C, 0x28}, //# Right MICPGA Gain is enabled, Right MICPGA Gain is set to 0dB 08
{0x00, 0x00}, //# Select Page 0
{0x53, 0x00}, //# Left ADC Channel Volume = 10dB 14
{0x54, 0x00}, //# Left ADC Channel Volume = 10dB 14
{0x51, 0xC0}, //# Power up LADC, Power up RADC
{0x52, 0x00}, //# Unmute LADC, Unmute RADC
};