This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3128 12脚 MUTE 供电问题



各位好,请帮忙看看TPA3128   MUTE这接线方式:

因为走线不好,所以MUTE取了GVDD,我看资料上的应用PIN2是取了GVDD,MUTE我也想取GVDD

如图,TPA3128的SDZ(PIN2,3)和MUTE(PIN12)取GVDD(PIN7)作供电控制,有问题么?

请帮忙确认一下。

  • MUTE I Mute signal for fast disable/enable of outputs (HIGH = outputs Hi-Z, LOW = outputs enabled). TTL logic levels with compliance to AVCC.

    这里要的是 TTL 逻辑电平. 可以看一下手册 6.3 Recommended Operating Conditions
  • 将mute,SDZ一直接在GVDD上,也就是一直为高电平,理论上TPA3128正常工作状态。
    可是,如果上电时,SDZ一直处于高电平容易产生POP声,我们是希望在上电时,SDZ处于低电平,当VCC电压全部起来之后再拉高,掉电也一样,希望SDZ置低,防止掉电时的POP声。