This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tlv320aic 3104 i2s —hpout 不出输出



 line in    hpout 输出正常  i2s 采集不输出 寄存器配置如下 {1, 0x80},
                {102, 0x02}, //c2
                {3, 0x81},
                {4, 0x20},
                {5, 0x0},
                {6, 0x0},
                {7, 0x8a},
                {8, 0x34},
                {9, 0x37},

                //{10, 0x01}, //offect
                {11, 0x01},
                {12, 0xff},  // dac 0xf0
                {15, 0x00}, //00
                {16, 0x00}, //00
                //in2lr
                {17, 0x0f}, //IN2l enable
                {18, 0xf0}, //IN2r LINE2 enable

                //in1lrlm
                //{19, 0x04}, //7c  // 4//LINE1L disable
                //{21, 0x80},
                //{22, 0x04}, //7c  // 4//LINE1R disable
                //{24, 0x80},
                {19, 0x04},   //MIC1LP/LINE1LP配置为单端模式  1:左ADC通道上电
                {21, 0x78},
                {22, 0x04},   //0:MIC1RP/LINE1RP配置为单端模式. 1:右ADC通道上电.
                {23, 0x78},
                {24, 0x78},

                {25, 0x40}, //00 micbias=2v  00

                {26, 0x00}, //00  adc 00ff Left AGC is enabled

                //{27, 0x00}, //fe adc off
                {28, 0x00}, //00
                {29, 0x00}, //00 adc off  

                //{30, 0x00}, //fe
                {31, 0x00}, //00

                {32, 0x00},
                {33, 0x00},
                //micbias
                //{25, 0x40}, //00 micbias=2v  00
                //agc未使能 26-36

                //dac
                {37, 0xc0},
                {38, 0x06},

                {40, 0xc0},
                //{41, 0x01},
                {41, 0x00},  //inl 2 adc1l , inr 2 adc1r, left adc volume and rigth adc volume have independent controle
                //dac path
                {42, 0xa8},
                {43, 0x00},
                {44, 0x00},

                {46, 0x80},  //00 //PGA_L to HPLOUT
                {47, 0x80}, //80  //hplout
                {51, 0x0d},  //0d

                {53, 0x80},//PGA_L to HPLCOM
                {54, 0x80}, //hplcom
                {58, 0x0d},

                {56, 0x80},    //PGA_R to HPLCOM Volume Control Register

                {57, 0x80},    //DAC_R1 to HPLCOM Volume Control Register
                {60, 0x80},  //PGA_L to HPROUT Volume Control Register
                {61, 0x80},   //DAC_L1 to HPROUT Volume Control Register


                {63, 0x80}, //00
                {64, 0x80}, //80 //hprout
                {65, 0x0d},

                {67, 0x80}, //PGA_L 到HPRCOM
                {68, 0x80},// :DAC_L1 到HPRCOM
                {70, 0x80}, //hprcom
                {71, 0x80}, //hprcom
                {72, 0x0d},
                {81, 0x80},

                {86, 0x09},  //0b